UDMA Low Level Driver API/interface data types file.
Go to the source code of this file.
Macros | |
#define | UDMA_CACHELINE_ALIGNMENT (128U) |
Cache line size for alignment of descriptor and buffers. More... | |
#define | UDMA_ALIGN_SIZE(x) (((x) + UDMA_CACHELINE_ALIGNMENT - 1U) & ~(UDMA_CACHELINE_ALIGNMENT - 1U)) |
Macro to align the size in bytes to UDMA cache line alignment. More... | |
#define | UDMA_DEFAULT_CH_DISABLE_TIMEOUT (100U) |
Default UDMA channel disable timeout. More... | |
UDMA Error Codes | |
#define | UDMA_SOK ( (int32_t) (0)) |
API call successful. More... | |
#define | UDMA_EFAIL (-(int32_t) (1)) |
API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure. More... | |
#define | UDMA_EBADARGS (-(int32_t) (2)) |
API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected. More... | |
#define | UDMA_EINVALID_PARAMS (-(int32_t) (3)) |
API call returned with error as invalid parameters. Typically when parameters passed are not valid or out of range. More... | |
#define | UDMA_ETIMEOUT (-(int32_t) (4)) |
API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period. More... | |
#define | UDMA_EALLOC (-(int32_t) (5)) |
API call returned with error as allocation failed. More... | |
UDMA Instance ID | |
This represents the various Instances in an SOC. The actual Instances present in the chip is SOC dependent. Refer soc file for the actual instance present. Kindly use Udma_InstanceIdSoc macros for SOC specific name. | |
#define | UDMA_INST_ID_0 (0U) |
#define | UDMA_INST_ID_1 (1U) |
#define | UDMA_INST_ID_2 (2U) |
#define | UDMA_INST_ID_3 (3U) |
UDMA Mapped Group | |
This represents the various Mapped TX & RX Channels/Rings in the SOC. The actual Mapped TX & RX groups present in the chip is SOC dependent. Refer soc file for the actual instance present. Kindly use Udma_MappedTxGrpSoc macros for Mapped TX SOC specific name and Udma_MappedRxGrpSoc macros for Mapped RX SOC specific name. | |
#define | UDMA_MAPPED_GROUP0 (0U) |
#define | UDMA_MAPPED_GROUP1 (1U) |
#define | UDMA_MAPPED_GROUP2 (2U) |
#define | UDMA_MAPPED_GROUP3 (3U) |
#define | UDMA_MAPPED_GROUP4 (4U) |
#define | UDMA_MAPPED_GROUP5 (5U) |
#define | UDMA_MAPPED_GROUP6 (6U) |
#define | UDMA_MAPPED_GROUP7 (7U) |
Typedefs | |
typedef void * | Udma_DrvHandle |
UDMA driver handle. More... | |
typedef void * | Udma_ChHandle |
UDMA channel handle. More... | |
typedef void * | Udma_EventHandle |
UDMA event handle. More... | |
typedef void * | Udma_RingHandle |
UDMA ring handle. More... | |
typedef void * | Udma_FlowHandle |
UDMA flow handle. More... | |