Request message to set keyrev.
This message can only be sent by the host that is tied to root of trust through the secure tisci_boardcfg extended otp extension
hdr | Standard TISCI header |
value | Key Revision value (integer) to be bit encoded, and programmed |
cert_addr_lo | Lower 32 bit address (in LE format) of the Dual signed certificate |
cert_addr_hi | Higher 32 bit address (in LE format) of the Dual signed certificate |
Data Fields | |
struct tisci_header | hdr |
uint32_t | value |
uint32_t | cert_addr_lo |
uint32_t | cert_addr_hi |
struct tisci_header tisci_msg_set_keyrev_req::hdr |
uint32_t tisci_msg_set_keyrev_req::value |
uint32_t tisci_msg_set_keyrev_req::cert_addr_lo |
uint32_t tisci_msg_set_keyrev_req::cert_addr_hi |