AM64x MCU+ SDK  09.00.00
management_address_tx_port_t Struct Reference

Data Fields

address_subtype_t address_subtype
 address_subtype:ipv4, ipv6 More...
 
char man_address [MAX_ADDRESS_LEN]
 man_address:192.168.88.109 More...
 
bool tx_enable
 
uint32_t addr_len
 
man_addr_if_subtype_t if_subtype
 
uint32_t if_id
 

Field Documentation

◆ address_subtype

address_subtype_t management_address_tx_port_t::address_subtype

address_subtype:ipv4, ipv6

◆ man_address

char management_address_tx_port_t::man_address[MAX_ADDRESS_LEN]

man_address:192.168.88.109

◆ tx_enable

bool management_address_tx_port_t::tx_enable

◆ addr_len

uint32_t management_address_tx_port_t::addr_len

◆ if_subtype

man_addr_if_subtype_t management_address_tx_port_t::if_subtype

◆ if_id

uint32_t management_address_tx_port_t::if_id