AM64x MCU+ SDK  09.00.00
SDL_VTM_tsGlobal_cfg Struct Reference

Detailed Description

VTM Global Configuration Registers.

This structure contains VTM Global Configuration register.

Data Fields

SDL_VTM_tsGlobal_ctrl_valid_map validMap
 
SDL_VTM_tsGlobal_clkSel clkSel
 
SDL_VTM_tsGlobal_clkDiv clkDiv
 
SDL_VTM_tsGlobal_any_maxt_outrg_alert_en any_maxt_outrg_alert_en
 
SDL_VTM_adc_code maxt_outrg_alert_thr0
 
SDL_VTM_adc_code maxt_outrg_alert_thr
 
SDL_VTM_tsGlobal_samples_per_count samplesPerCnt
 

Field Documentation

◆ validMap

SDL_VTM_tsGlobal_ctrl_valid_map SDL_VTM_tsGlobal_cfg::validMap

valid bit map for temperature sensor global control

◆ clkSel

SDL_VTM_tsGlobal_clkSel SDL_VTM_tsGlobal_cfg::clkSel

Temperature sensor clock source selector. 0 = fix_ref_clk as source. 1 = fix_ref2_clk as source

◆ clkDiv

SDL_VTM_tsGlobal_clkDiv SDL_VTM_tsGlobal_cfg::clkDiv

Temperature sensor clock source divider selector. Default set by e-fuse or tie-off. Divider uses select reference clock as source. 0 = 1x divide. 1 = 2x divide. ... 15 = 16x divide. ... 63 = 64x divide.

◆ any_maxt_outrg_alert_en

SDL_VTM_tsGlobal_any_maxt_outrg_alert_en SDL_VTM_tsGlobal_cfg::any_maxt_outrg_alert_en

This bit in VTM_MISC_CTRL register, when enable will cause, the VTM’s output therm_maxtemp_outrange_alert to be driven high, if any of the sources for the MAXT_OUTRG_ALERT, is set high.

◆ maxt_outrg_alert_thr0

SDL_VTM_adc_code SDL_VTM_tsGlobal_cfg::maxt_outrg_alert_thr0

ADC code programmed in VTM_MISC_CTRL2 for the global max temperature out of range safe sample value. If the alert is enabled globally for the sensor, and the sensor reads a value <= this value, then the alert is cleared after being triggered

◆ maxt_outrg_alert_thr

SDL_VTM_adc_code SDL_VTM_tsGlobal_cfg::maxt_outrg_alert_thr

ADC code programmed in VTM_MISC_CTRL2 for the global max temperature out of range sample value. If the alert is enabled globally for the sensor, and the sensor reads a value >= this value, then the alert is triggered

◆ samplesPerCnt

SDL_VTM_tsGlobal_samples_per_count SDL_VTM_tsGlobal_cfg::samplesPerCnt

Temperature sensor sample period count selector, programmed in VTM_SAMPLE_CTRL reg