AM64x MCU+ SDK  09.00.00
Enet_IoctlValidate Struct Reference

Detailed Description

Enet IOCTL expected param sizes.

Expected input and output argument sizes of an Enet IOCTL. This is useful for validation purposes only.

Data Fields

uint32_t cmd
 
uint32_t inArgsSize
 
uint32_t outArgsSize
 

Field Documentation

◆ cmd

uint32_t Enet_IoctlValidate::cmd

Command id

◆ inArgsSize

uint32_t Enet_IoctlValidate::inArgsSize

Expected size of IOCTL input argument (Enet_IoctlPrms.inArgsSize)

◆ outArgsSize

uint32_t Enet_IoctlValidate::outArgsSize

Expected size of IOCTL output argument (Enet_IoctlPrms.outArgsSize)