AM64x MCU+ SDK  09.00.00
APIs for MMU for ARMv8 (ARM A53)

Introduction

For more details and example usage, see MMU for ARMv8 (ARM A53)

Data Structures

struct  MmuP_MapAttrs
 Attribute's to apply for a MMU region. More...
 
struct  MmuP_Config
 MMU config structure, this used by SysConfig and not to be used by end-users directly. More...
 
struct  MmuP_RegionConfig
 Region config structure, this used by SysConfig and not to be used by end-users directly. More...
 

Functions

void MmuP_MapAttrs_init (MmuP_MapAttrs *attrs)
 Set default values to MmuP_MapAttrs. More...
 
void MmuP_enable (void)
 Enable MMU sub-system. More...
 
void MmuP_disable (void)
 Disable MMU sub-system. More...
 
uint32_t MmuP_isEnabled (void)
 Check if MMU sub-system is enabled. More...
 
int32_t MmuP_map (uintptr_t vaddr, uintptr_t paddr, uint32_t size, MmuP_MapAttrs *mapAttrs)
 Setup a region in the MMU. More...
 
void MmuP_init (void)
 Initialize MMU sub-system, called by SysConfig, not to be called by end users. More...
 

Enumerations

enum  MmuP_AccessPerm { MMUP_ACCESS_PERM_PRIV_RW_USER_NONE = 0x0, MMUP_ACCESS_PERM_PRIV_RW_USER_RW = 0x1, MMUP_ACCESS_PERM_PRIV_RO_USER_NONE = 0x2, MMUP_ACCESS_PERM_PRIV_RO_USER_RO = 0x3 }
 Enum's to represent different types of access permissions that are possible for a given MMU region. More...
 
enum  MmuP_Shareable { MMUP_SHARABLE_NONE = 0x0, MMUP_SHARABLE_OUTER = 0x2, MMUP_SHARABLE_INNER = 0x3 }
 Enum's to represent MMU region sharable status. More...
 
enum  MmuP_AttrIndx {
  MMUP_ATTRINDX_MAIR0 = 0, MMUP_ATTRINDX_MAIR1, MMUP_ATTRINDX_MAIR2, MMUP_ATTRINDX_MAIR3,
  MMUP_ATTRINDX_MAIR4, MMUP_ATTRINDX_MAIR5, MMUP_ATTRINDX_MAIR6, MMUP_ATTRINDX_MAIR7
}
 Enum's to represent MMU attribute index. More...
 

Enumeration Type Documentation

◆ MmuP_AccessPerm

Enum's to represent different types of access permissions that are possible for a given MMU region.

Enumerator
MMUP_ACCESS_PERM_PRIV_RW_USER_NONE 

RW Permission in privileged mode only

MMUP_ACCESS_PERM_PRIV_RW_USER_RW 

RW Permission in privileged and user mode

MMUP_ACCESS_PERM_PRIV_RO_USER_NONE 

RD Permission for privileged mode and access bllocked for user mode

MMUP_ACCESS_PERM_PRIV_RO_USER_RO 

All access are blocked

◆ MmuP_Shareable

Enum's to represent MMU region sharable status.

Enumerator
MMUP_SHARABLE_NONE 

Not shareable

MMUP_SHARABLE_OUTER 

Outer shareable

MMUP_SHARABLE_INNER 

Inner shareable

◆ MmuP_AttrIndx

Enum's to represent MMU attribute index.

Enumerator
MMUP_ATTRINDX_MAIR0 
MMUP_ATTRINDX_MAIR1 
MMUP_ATTRINDX_MAIR2 
MMUP_ATTRINDX_MAIR3 
MMUP_ATTRINDX_MAIR4 
MMUP_ATTRINDX_MAIR5 
MMUP_ATTRINDX_MAIR6 
MMUP_ATTRINDX_MAIR7 

Function Documentation

◆ MmuP_MapAttrs_init()

void MmuP_MapAttrs_init ( MmuP_MapAttrs attrs)

Set default values to MmuP_MapAttrs.

Strongly recommended to be called before seting values in MmuP_MapAttrs

Parameters
attrs[out] parameter structure to set to default

◆ MmuP_enable()

void MmuP_enable ( void  )

Enable MMU sub-system.

◆ MmuP_disable()

void MmuP_disable ( void  )

Disable MMU sub-system.

◆ MmuP_isEnabled()

uint32_t MmuP_isEnabled ( void  )

Check if MMU sub-system is enabled.

Returns
0: MMU sub-system is disabled, 1: MMU sub-system is enabled

◆ MmuP_map()

int32_t MmuP_map ( uintptr_t  vaddr,
uintptr_t  paddr,
uint32_t  size,
MmuP_MapAttrs mapAttrs 
)

Setup a region in the MMU.

Note
Recommended to disable MMU and disable cache before setting up MMU regions
Parameters
vaddr[in] virtual address of region to setup, MUST aligned to granule size
paddr[in] physical address of region to setup, MUST aligned to granule size
size[in] region size, MUST aligned to granule size
mapAttrs[in] map attrs, see MmuP_MapAttrs

◆ MmuP_init()

void MmuP_init ( void  )

Initialize MMU sub-system, called by SysConfig, not to be called by end users.