AM64x MCU+ SDK  09.00.00
enet_osal_dflt.h File Reference

Introduction

This file contains the default OSAL implementation interface.

Go to the source code of this file.

Functions

void EnetOsalDflt_initCfg (EnetOsal_Cfg *cfg)
 Initialize EnetOsal config with PDK OSAL-based default implementation. More...
 

Function Documentation

◆ EnetOsalDflt_initCfg()

void EnetOsalDflt_initCfg ( EnetOsal_Cfg cfg)

Initialize EnetOsal config with PDK OSAL-based default implementation.

Initializes the OSAL configuration parameters with a default implementation based on PDK OSAL layer.

Parameters
cfgPointer to the initialization parameters to be initialized