Introduction
This Enet TSN example illustrates the usage of gPTP 802.1AS stack with CPSW peripheral. The application illustrates the following
- gPTP EndPoint slave mode
- gPTP EndPoint master mode
- gPTP Switch mode
Yang based configuration is also supported. Currently File System is not supported, will be added in future releases. In this example, We use two Rx and two Tx DMA channel, one Rx and one Tx channel specific to gPTP traffic. All the non-PTP traffic is handled on the other DMA channel in a echo task.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0_freertos |
Toolchain | ti-arm-clang |
Board | am64x-evm |
Example folder | examples/networking/tsn/gptp_app |
Steps to Run the Example
Build the example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
HW Setup
- Note
- Make sure you have setup the EVM with cable connections as shown here, EVM Setup. In addition do below steps.
AM64X-EVM
For CPSW based example
- Connect a ethernet cable to the EVM from host PC as shown below. If you have multiple boards, you can connect both of them and run the same application on both the boards.
Ethernet cable for CPSW based ethernet
Run the example
- Attention
- If you need to reload and run again, a CPU power-cycle is MUST
- Launch a CCS debug session and run the example executable, see CCS Launch, Load and Run
- You can either use two boards connected to each other and run the example on both of them. Or you can connect to a linux PC as other PTP instance. Please make sure your linux PC has a gPTP capable network card.
- If you are connecting the board to a linux PC. You should use the ptp4l gptp config https://github.com/richardcochran/linuxptp/blob/master/configs/gPTP.cfg on the linux.
- Command on Linux:
sudo ptp4l -i eno1 -m -l 6 -q -f ~/gptp_config.cfg
-i <interface name> -f <path to cfg file>
- For some network cards, there is a bug with prop delay. So, you might need to increase the neighborPropDelayThresh in that case as below.
[global]
gmCapable 1
priority1 248
priority2 248
logAnnounceInterval 0
logSyncInterval -3
syncReceiptTimeout 3
neighborPropDelayThresh 10000
min_neighbor_prop_delay -20000000
assume_two_step 1
path_trace_enabled 1
follow_up_info 1
transportSpecific 0x1
ptp_dst_mac 01:80:C2:00:00:0E
network_transport L2
delay_mechanism P2P
priority1
can be changed to make the linux PC master or slave. Lower the number higher the priority to become master.
- You will see logs in the UART terminal as shown in the next section. The linux PC side logs are with intel i210 card.
Sample output for Enet gPTP example
- Linux PC as gPTP slave and DUT as gPTP master
==========================
gPTP App
==========================
Enabling clocks!
sitara-cpsw: Create RX task for regular traffic
start to open driver.
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:1 From 4 To 2
Init all configs
----------------------------------------------
sitara-cpsw: init config
Mdio_open:294
sitara-cpsw: Open port 1
EnetPhy_bindDriver:1717
sitara-cpsw: Open port 2
EnetPhy_bindDriver:1717
PHY 0 is alive
PHY 3 is alive
initQs() txFreePktInfoQ initialized with 16 pkts
MAC port addr: 34:08:e1:80:a9:36
unibase-1.1.5
app_start:gptp start done!
INF:def04:simpledb_open:no data is imported
INF:def04:uc_hwal_open:
INF:cbase:cb_rawsock_open:dmaTxChId=0 dmaRxChId=0 nTxPkts=16 nRxPkts=32 pktSize=1536
INF:cbase:Mac addr has not been allocated
INF:def04:000000-083173:uniconf_main:uniconf started
gptp_task: started.
gptp_task: dbname=INF:def04:get_exmodid_in_db:first xl4gptp:exmodid=0
INF:gptp:gptpman_run:max_domains=1, max_ports=2
INF:cbase:cb_rawsock_open:dmaTxChId=1 dmaRxChId=1 nTxPkts=16 nRxPkts=32 pktSize=1536
INF:cbase:Mac addr has not been allocated
INF:gptp:dev:tilld0 open success
INF:gptp:dev:tilld1 open success
INF:gptp:gptpnet_init:Open lldtsync OK!
INF:gptp:IEEE1588-2019 performance monitoring enabled.
INF:gptp:onenet_activate:tilld0 status=0, duplex=0, speed=0Mbps
INF:gptp:onenet_activate:tilld1 status=0, duplex=0, speed=0Mbps
INF:gptp:000000-250060:domainIndex=0, GM changed old=00:00:00:00:00:00:00:00, new=34:08:E1:FF:FE:80:A9:36
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2
INF:gptp:set_phase_offsetGM:domainIndex=0, New adjustment(New GM?)
Cpsw_handleLinkUp:1449
MAC Port 1: link up
INF:gptp:index=1 speed=1000, duplex=full, ptpdev=tilld0
INF:gptp:md_pdelay_resp_sm_recv_req:port=1, set receivedNonCMLDSPdelayReq=1
5. 61s : CPU load = 5.54 %
WRN:gptp:000005-750522:waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=68:05:CA:FF:FE:C8:7A:C2, thisClock=34:08:E1:FF:FE:80:A9:36, neighborPropDelay=215
INF:gptp:waiting_for_pdelay_interval_timer_proc:portIndex=1, not asCapable
INF:gptp:waiting_for_pdelay_interval_timer_proc:set asCapableAcrossDomains, portIndex=1
INF:gptp:set asCapable for domainIndex=0, portIndex=1
INF:gptp:000006-759636:gptpgcfg_set_asCapable:domainInde=0, portIndex=1, ascapable=1
INF:gptp:000006-767874:gm_stable:gm_unstable_proc:domainIndex=0
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1
INF:gptp:000006-779474:gm_stable:gm_unstable_proc:domainIndex=0
INF:gptp:000006-874385:setSyncTwoStep_txSync:domainIndex=0, portIndex=1, sync gap=6874msec
INF:gptp:000006-879953:setFollowUp_txFollowUp:domainIndex=0, portIndex=1, fup gap=6879msec
INF:gptp:000007-874661:gm_stable:gm_stable_proc:domainIndex=0
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
10. 63s : CPU load = 4.40 %
15. 64s : CPU load = 4.01 %
20. 65s : CPU load = 4.14 %
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
25. 66s : CPU load = 4.03 %
30. 67s : CPU load = 4.13 %
domain=0, offset=0nsec, hw-adjrate=0ppb
gmsync=true, last_setts64=0nsec
ptp4l[302.853]: selected /dev/ptp0 as PTP clock
ptp4l[302.924]: port 1: INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[302.924]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[306.578]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[306.578]: selected local clock 6805ca.fffe.c87ac2 as best master
ptp4l[306.578]: assuming the grand master role
ptp4l[306.830]: port 1: new foreign master 3408e1.fffe.80a936-1
ptp4l[308.831]: selected best master clock 3408e1.fffe.80a936
ptp4l[308.831]: port 1: MASTER to UNCALIBRATED on RS_SLAVE
ptp4l[309.209]: port 1: UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
ptp4l[309.831]: rms 846011109112972288 max 1692022218225946112 freq -44595 +/- 20153 delay 201 +/- 0
ptp4l[310.831]: rms 3739 max 5721 freq -35541 +/- 5086 delay 201 +/- 0
ptp4l[311.830]: rms 6234 max 6535 freq -24176 +/- 1658 delay 200 +/- 0
ptp4l[312.831]: rms 3966 max 5256 freq -21940 +/- 152 delay 200 +/- 0
ptp4l[313.831]: rms 1297 max 2132 freq -23123 +/- 456 delay 199 +/- 0
ptp4l[314.830]: rms 220 max 340 freq -24465 +/- 287 delay 200 +/- 0
ptp4l[315.830]: rms 355 max 378 freq -25088 +/- 84 delay 199 +/- 0
ptp4l[316.830]: rms 211 max 285 freq -25184 +/- 16 delay 199 +/- 0
ptp4l[317.830]: rms 59 max 103 freq -25096 +/- 31 delay 199 +/- 0
ptp4l[318.830]: rms 27 max 38 freq -25002 +/- 22 delay 199 +/- 0
ptp4l[319.830]: rms 37 max 42 freq -24950 +/- 12 delay 199 +/- 0
ptp4l[320.830]: rms 28 max 35 freq -24928 +/- 6 delay 199 +/- 0
ptp4l[321.830]: rms 20 max 27 freq -24914 +/- 6 delay 200 +/- 0
ptp4l[322.830]: rms 13 max 17 freq -24906 +/- 5 delay 200 +/- 0
ptp4l[323.830]: rms 15 max 17 freq -24888 +/- 3 delay 200 +/- 0
ptp4l[324.830]: rms 13 max 17 freq -24877 +/- 6 delay 200 +/- 0
ptp4l[325.830]: rms 15 max 20 freq -24859 +/- 7 delay 201 +/- 0
ptp4l[326.830]: rms 18 max 20 freq -24839 +/- 7 delay 201 +/- 0
ptp4l[327.830]: rms 14 max 18 freq -24827 +/- 7 delay 201 +/- 0
- Linux PC as gPTP master and DUT as gPTP slave
ptp4l[480.714]: selected /dev/ptp0 as PTP clock
ptp4l[480.772]: port 1: INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[480.772]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE
ptp4l[483.492]: port 1: link down
ptp4l[483.492]: port 1: LISTENING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)
ptp4l[483.507]: selected local clock 6805ca.fffe.c87ac2 as best master
ptp4l[483.507]: assuming the grand master role
ptp4l[486.452]: port 1: link up
ptp4l[486.524]: port 1: FAULTY to LISTENING on INIT_COMPLETE
ptp4l[490.210]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
ptp4l[490.211]: selected local clock 6805ca.fffe.c87ac2 as best master
ptp4l[490.211]: assuming the grand master role
==========================
gPTP App
==========================
Enabling clocks!
sitara-cpsw: Create RX task for regular traffic
start to open driver.
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:1 From 4 To 2
Init all configs
----------------------------------------------
sitara-cpsw: init config
Mdio_open:294
sitara-cpsw: Open port 1
EnetPhy_bindDriver:1717
sitara-cpsw: Open port 2
EnetPhy_bindDriver:1717
PHY 0 is alive
PHY 3 is alive
initQs() txFreePktInfoQ initialized with 16 pkts
MAC port addr: 34:08:e1:80:a9:36
unibase-1.1.5
app_start:gptp start done!
INF:def04:simpledb_open:no data is imported
INF:def04:uc_hwal_open:
INF:cbase:cb_rawsock_open:dmaTxChId=0 dmaRxChId=0 nTxPkts=16 nRxPkts=32 pktSize=1536
INF:cbase:Mac addr has not been allocated
INF:def04:000000-083207:uniconf_main:uniconf started
gptp_task: started.
gptp_task: dbname=INF:def04:get_exmodid_in_db:first xl4gptp:exmodid=0
INF:gptp:gptpman_run:max_domains=1, max_ports=2
INF:cbase:cb_rawsock_open:dmaTxChId=1 dmaRxChId=1 nTxPkts=16 nRxPkts=32 pktSize=1536
INF:cbase:Mac addr has not been allocated
INF:gptp:dev:tilld0 open success
INF:gptp:dev:tilld1 open success
INF:gptp:gptpnet_init:Open lldtsync OK!
INF:gptp:IEEE1588-2019 performance monitoring enabled.
INF:gptp:onenet_activate:tilld0 status=0, duplex=0, speed=0Mbps
INF:gptp:onenet_activate:tilld1 status=0, duplex=0, speed=0Mbps
INF:gptp:000000-250054:domainIndex=0, GM changed old=00:00:00:00:00:00:00:00, new=34:08:E1:FF:FE:80:A9:36
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2
INF:gptp:set_phase_offsetGM:domainIndex=0, New adjustment(New GM?)
Cpsw_handleLinkUp:1449
MAC Port 1: link up
INF:gptp:index=1 speed=1000, duplex=full, ptpdev=tilld0
WRN:gptp:000003-535968:waiting_for_pdelay_resp_condition:sequenceId doesn't match, expected=6097, received=6096
WRN:gptp:000003-542863:waiting_for_pdelay_resp_condition:Discard this RESP and wait for the next one, this could be because of SM Reset. SeqId: expected=6097, received=6096
WRN:gptp:000003-557981:waiting_for_pdelay_resp_follow_up_condition:portIndex=1, sequenceId doesn't match, expected=6097, received=6096
WRN:gptp:000003-569875:waiting_for_pdelay_resp_follow_up_condition:portIndex=1, PdelayResp comes twice for the same PdelayReq, sequenceId=6097
WRN:gptp:000004-499985:waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=68:05:CA:FF:FE:C8:7A:C2, thisClock=34:08:E1:FF:FE:80:A9:36, neighborPropDelay=207
INF:gptp:waiting_for_pdelay_interval_timer_proc:portIndex=1, not asCapable
INF:gptp:md_pdelay_resp_sm_recv_req:port=1, set receivedNonCMLDSPdelayReq=1
5. 61s : CPU load = 5.59 %
INF:gptp:waiting_for_pdelay_interval_timer_proc:set asCapableAcrossDomains, portIndex=1
INF:gptp:set asCapable for domainIndex=0, portIndex=1
INF:gptp:000005-509628:gptpgcfg_set_asCapable:domainInde=0, portIndex=1, ascapable=1
INF:gptp:000005-517856:gm_stable:gm_unstable_proc:domainIndex=0
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1
INF:gptp:000005-529441:gm_stable:gm_unstable_proc:domainIndex=0
INF:gptp:000005-624384:setSyncTwoStep_txSync:domainIndex=0, portIndex=1, sync gap=5624msec
INF:gptp:000005-629953:setFollowUp_txFollowUp:domainIndex=0, portIndex=1, fup gap=5629msec
INF:gptp:000006-624596:gm_stable:gm_stable_proc:domainIndex=0
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2
INF:gptp:000007-223644:domainIndex=0, GM changed old=34:08:E1:FF:FE:80:A9:36, new=68:05:CA:FF:FE:C8:7A:C2
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=0
INF:gptp:000007-237037:gm_stable:gm_unstable_proc:domainIndex=0
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1
INF:gptp:set_phase_offsetGM:domainIndex=0, New adjustment(New GM?)
INF:gptp:set_phase_offsetGM:domainIndex=0, offset adjustment, diff=-779404313
INF:gptp:set_phase_offsetGM:domainIndex=0, stable
INF:gptp:clock_master_sync_receive:computeGmRateRatio:domainIndex=0 unstable rate=802ppb (timeleap_future)
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 1907ppb, GMdiff=11052nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 3750ppb, GMdiff=12284nsec
domain=0, offset=0nsec, hw-adjrate=3750ppb
gmsync=true, last_setts64=0nsec
10. 62s : CPU load = 4.59 %
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 5495ppb, GMdiff=13149nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 7126ppb, GMdiff=13678nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 8610ppb, GMdiff=13873nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 9945ppb, GMdiff=13785nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 11111ppb, GMdiff=13430nsec
15. 63s : CPU load = 4.45 %
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 12110ppb, GMdiff=12856nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 12926ppb, GMdiff=12072nsec
INF:gptp:000017-249245:gm_stable:gm_stable_proc:domainIndex=0
INF:gptp:gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 13577ppb, GMdiff=11144nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 14061ppb, GMdiff=10091nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 14384ppb, GMdiff=8947nsec
20. 64s : CPU load = 4.58 %
domain=0, offset=0nsec, hw-adjrate=14384ppb
gmsync=true, last_setts64=0nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 14556ppb, GMdiff=7741nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 14591ppb, GMdiff=6507nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 14504ppb, GMdiff=5277nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 14307ppb, GMdiff=4068nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 14015ppb, GMdiff=2901nsec
25. 65s : CPU load = 4.48 %
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 13649ppb, GMdiff=1805nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 13649ppb, GMdiff=1805nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 13217ppb, GMdiff=783nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 12739ppb, GMdiff=-148nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 12231ppb, GMdiff=-971nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to 11702ppb, GMdiff=-1693nsec
30. 66s : CPU load = 4.56 %
TSN Stack
This guide is intended to enhance user's understanding of the TSN stack and provide guidance on how to seamlessly integrate TSN modules into their own applications.
TSN source modules
The TSN library is composed of the following source modules:
- tsn_unibase: Universal utility libraries that are platform-independent.
- tsn_combase: Communication utility libraries that provide support for functions like sockets, mutexes, and semaphores.
- tsn_uniconf: Universal configuration daemon for Yang, provides APIs for developing a client application which retreives/writes yang parameters from/to database and ask the uniconf for configurating HW.
- tsn_gptp: Implementation of the IEEE 802.1 AS gptp protocol.
TSN Initialization
A reference of the TSN stack initialization can be found in <mcu_plus_sdk>/examples/networking/tsn/gptp_app/tsninit.c
. Prior to any module calls, it is necessary to initialize the unibase library once. This can be achieved by invoking the tsn_init()
function.
TSN Logging
By default, TSN logs are directed to STDOUT using the fwrite function: fwrite(str, 1, strlen(str), stdout);
However, it is possible to customize the log output by setting the console_out
callback during the initialization of the unibase library in the tsn_init()
function.
When a callback function is assigned to console_out
it takes a significant amount of time to log to the output device, it is advisable to log to a buffer and utilize another task to log from the buffer to the desired output device. This approach helps to prevent log delays that could adversely affect the gPTP task, such as incorrect Sync and FollowUp intervals. The option to log to a buffer is supported when the TSN_USE_LOG_BUFFER
macro is defined.
To enable specific log levels, you can modify the ub_log_initstr parameter in the tsn_init() function. There are eight log levels available::
UBL_NONE = 0
UBL_FATAL = 1
UBL_ERROR = 2
UBL_WARN = 3
UBL_INFO = 4
UBL_INFOV = 5
UBL_DEBUG = 6
UBL_DEBUGV = 7
For example: init_para.ub_log_initstr = "4,ubase:45,cbase:45,gptp:55,uconf:45";
In the above example, uconf:45
signifies the following:
4 (INFO)
: Log level for printing to the console. 5 (INFOV)
: Log level for storing in internal memory (which can be dumped to a file).
Please note that enabling the DEBUG or DEBUGV level will result in a large number of logs being generated. If the log buffer is used, it may overflow, causing some logs to be lost.
The first '4' character in "4,ubase...
represents the default log level applied to all modules.
Starting uniconf and gPTP
The gPTP functionality operates in a separate task, alongside the universal configuration daemon "uniconf". To start these tasks, use the tsn_app_start()
in tsninit.c as reference .
This function will start the uniconf and gPTP tasks.
TSN Deinitialization
To deinitialize the TSN modules, you can invoke the tsn_app_stop();
and tsn_app_deinit();
functions.
Integration
Source integration
To integrate the TSN stack into your application, follow these steps:
Initialize Enet LLD and setup board dependencies. In the TSN example application, the initialization routines can be found at <mcu_plus_sdk>/examples/networking/tsn/gptp_app/tsnapp_main.c
, which can be used as reference.
The main functions related to EVM board initialization are::
EnetAppUtils_enableClocks();
EnetApp_driverInit();
EnetApp_driverOpen();
...
These functions are responsible for configuring pinmux, GPIOs, etc., as well as providing the MAC port and PHY configuration parameters, which are board specific.
- Before calling any TSN module APIs, ensure you initialize TSN by calling
tsn_app_init()
.
- Initialize the combase Ethernet device table as the following code snippet::
for (i = 0; i < numEthPorts; i++)
{
snprintf(&gEnetApp_gPtpNetDevs[i][0], IFNAMSIZ, "tilld%d", i);
/* ethdevs[i].netdev must hold a global address, not a stack address */
ethdevs[i].netdev = gEnetApp_gPtpNetDevs[i];
ethdevs[i].macport = ethPorts[i].macPort;
}
cb_lld_init_devs_table(ethdevs, i, enetType, instId);
In the above code, the Ethernet device name is not mandatory but it's useful as a virtual Ethernet device table that facilitates the conversion between the device name and the MAC port number.
Please ensure that the ethdevs[i].netdev
pointer points to a global memory location rather than a stack memory. The combase layer will reference this address instead of making a copy.
- To provide syscfg values to the TSN stack, you can use the
cb_socket_set_lldcfg_update_cb()
`
- Start the gPTP task by calling
tsn_app_start()
. This will start the necessary threads for gPTP and uniconf.
Uniconf configuration
Universal configuration daemon for Yang, provides APIs for developing a client application which retreives/writes yang parameters from/to database and ask the uniconf for configurating HW.
Uniconf supports the following config paramaters:
typedef struct ucman_data {
const char *dbname;
const char **configfiles;
int numconfigfile;
uint8_t ucmode;
bool *stoprun;
int rval;
UC_NOTICE_SIG_T *ucmanstart;
const char *hwmod;
} ucman_data_t;
dbname
: Specify the path of database file in the file system. If user wants to write all config parameters to database file to make the config parameter persist after a reboot, the full path of database file must be set via this parameter. Currently, as file system is not supported, this parameter is set to NULL
.
configfiles
: array of runtime config files will be used by the uniconf. Run time config file is a text file which has one-to-one mapping with yang files, the format of each line of a run time config file is specified under <mcu_plus_sdk>/source/networking/tsn/tsn-stack/tsn_uniconf/README.org
. Currently, as file system is not supported, this parameter is set to NULL
.
numofconfigfile
: Specify how many config files have been set via the the configfiles
array above. Currently, this parameter is set to 0
.
ucmode
: This is for setting the expected mode of uniconf. The uniconf can only run in a separated thread, please set UC_CALLMODE_THREAD|UC_CALLMODE_UNICONF
for this parameter.
stoprun
: Address to a flag which signals the uniconf to stop in case the flag is true.
rval
: Error code of the uniconf in case error occurs.
ucmanstart
: The name of semaphore or a semaphore object in case of FreeRTOS. If this parameter is not NULL
, the uniconf will post this semaphore to signal application layer indicating that it has been started successfully.
hwmod
: Configure the HW for the uniconf. If an empty string is specified (hwmod=""), it means the uniconf will configure HW. If "NONE" is specified (hwmod="NONE"), the uniconf will not configure HW when client side writes the database and ask it for an update.
gPTP Yang Parameters
This section describes the yang parameters used for gPTP. These parameters are described in the file: standard/ieee/draft/1588/ieee1588-ptp.yang of the repository: https://github.com/YangModels/yang.git
underlying-interface
: Named reference to a configured ptp port.
port-enable
: Enable or disable the port. If the port is disabled, it will not be used for synchronization.
log-announce-interval
: The logarithm to the base 2 of the announce interval in seconds. The default value is 0, which corresponds to 1 second for the announce interval.
gptp-cap-receipt-timeout
: Number of transmission intervals that a port waits without receiving the gPTP capable message before it is determined to not run gPTP.
announce-receipt-timeout
: The number of times an announce interval must pass without receiving an announce message before the port is considered faulty. The default value is 3.
log-sync-interval
: The logarithm to the base 2 of the sync interval in seconds. The default value is -3, which corresponds to 125ms for the sync interval.
minor-version-number
: The minor version number of the gPTP protocol. The default value is 1.
initial-log-announce-interval
: The logarithm to the base 2 of the initial announce interval. The default value is 0, which corresponds to 1 second for the announce interval.
sync-receipt-timeout
: The number of sync intervals to must pass without receiving a sync message before the port is considered faulty. The default value is 3.
initial-log-sync-interval
: The logarithm to the base 2 of the initial sync interval. The default value is -3, which corresponds to 125ms for the sync interval.
current-log-sync-interval
: The logarithm to the base 2 of the current sync interval. The default value is -3, which corresponds to 125ms for the sync interval.
current-log-gptp-cap-interval
: The logarithm to the base 2 of the gPTP capable messages interval. The default value is 3, which corresponds to 8 seconds.
initial-log-pdelay-req-interval
: The logarithm to the base 2 of the initial pdelay request interval. The default value is 0, which corresponds to 1 second for the pdelay request.
current-log-pdelay-req-interval
: The logarithm to the base 2 of the current pdelay request interval. The default value is 0, which corresponds to 1 second for the pdelay request.
allowed-lost-responses
: The number of consecutive pdelay request intervals with no pdelay response that the port can miss before it is considered faulty. The default value is 9.
allowed-faults
: The number of faults above with asCapable is set to false. The default value is 9.
mean-link-delay-thresh
: The Propagation time threshold to consider that a linked port is not asCapable. The default value is 0x27100000, which corresponds to 10000<<16, 10000nsec.
priority1
: The priority1 of the PTP instance, used in the best master clock algorithm. The default value is 250.
external-port-config-enable
: Enable or disable the external port configuration. This is set by default as false, to have the port state determined by the gPTP protocol.
time-source
: The time source of the PTP instance. The default value is "internal-oscillator".
ptp-timescale
: The PTP timescale of the PTP instance. The default value is true, having the timescale of the Grandmaster PTP instance is PTP.
gPTP configuration
There are following types of yang config parameters for gPTP:
- Config parameters which belong to yang standard as described above, can be referred from
(github.com/YangModels/yang.git): ieee1588-ptp.yang, ieee802-dot1as-ptp.yang, etc. (gptp-yangconfig.xml in source/networking/tsn/tsn-stack/tsn_gptp/gptpconf/)
- Non-yang config parameters which are parameters needed for the gPTP but they are
not defined in the yang standard. (gptp_nonyangconfig.xml in source/networking/tsn/tsn-stack/tsn_gptp/gptpconf/)
To configure gPTP, you can set/read the values of yang parameters during runtime by using the API yang_db_runtime_put_oneline (see the tsninit.c), yang_db_runtime_get_oneline for retrieving values and similarly for non-yang params these are the APIs gptpgcfg_set_item()
to set, gptpgcfg_get_item
to retreive, with prototype :
int gptpgcfg_set_item(uint8_t gptpInstanceIndex, uint8_t confitem,
bool status, void *value, uint32_t vsize);
gptpInstanceIndex
: Index of the gptp to be configured. For RTOS, because only one instance is applicable, should be set to 0.
confitem
: From the desired parameter in gptp_nonyangconfig.xml in source/networking/tsn/tsn-stack/tsn_gptp/gptpconf/ (Note: these xml files are only used for internal code generation), Add XL4_EXTMOD_XL4GPTP
prefix to the param name with underscores as delimiter.
- For instance, within the gptp_nonyangconfig.xml,
USE_HW_PHASE_ADJUSTMENT
will have an equivalent XL4_EXTMOD_XL4GPTP_USE_HW_PHASE_ADJUSTMENT
.
status
: YDBI_CONFIG
or YDBI_STATUS
. YDBI_CONFIG
is used to configure the parameter at runtime. YDBI_STATUS
is used to configure the parameter at runtime and store the value in the database for persistence.
value
: Pointer to the value to be set.
vsize
: Size of the value to be set, for the items.
Example usage: gptpgcfg_set_item(gpoptd.instnum, XL4_EXTMOD_XL4GPTP_USE_HW_PHASE_ADJUSTMENT, YDBI_CONFIG, &use_hwphase, sizeof(use_hwphase));
- As a reference, please consult the
<mcu_plus_sdk>/examples/networking/tsn/gptp_app/tsninit.c
file.
- The configuration must be done before calling the
gptpman_run()
function inside the tsninit.c
file, after the gptpgcfg_init function call.
gPTP Performance optimization
Out of box configuration is not optimized for performance as the connected devices (like some intel cards) may not be compatible with these optimal configuration. The following configurations can be tuned for optimizing the gPTP performance:
XL4_EXTMOD_XL4GPTP_CLOCK_COMPUTE_INTERVAL_MSEC
: The interval in milliseconds at which the gPTP clock is computed. The default value is currently set to 1000
, and has a parameter vsize of 1
(uint8_t).
XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_UPDATE_MRATE_PPB
: The rate at which the frequency offset is updated. The default value is currently set to 10
, and has a parameter vsize of 4
(uint32_t).
XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_STABLE_VALUE
: The reciprocal of this is the alpha value of the IIR filter used to compute the phase offset. The default value is currently set to 10
, and has a parameter vsize of 4
(uint32_t).
XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_STABLE_VALUE
: The reciprocal of this is the alpha value of the IIR filter used to compute the frequency offset. The default value is currently set to 10
, and has a parameter vsize of 4
(uint32_t).
e.g. The following is an example configuration which you can use in the example to get better accuaracy if compatible with your devices in the setup. The following configuration is tested with intel i210 card and in between two EVMs.
uint8_t compute_interval = 100;
uint32_t freq_offset_update_mrate_ppb = 5;
uint32_t phase_offset_iir_alpha_stable_value = 1;
uint32_t freq_offset_iir_alpha_stable_value = 2;
gptpgcfg_set_item(gpoptd.instnum, XL4_EXTMOD_XL4GPTP_CLOCK_COMPUTE_INTERVAL_MSEC, YDBI_CONFIG, &compute_interval, sizeof(compute_interval));
gptpgcfg_set_item(gpoptd.instnum, XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_UPDATE_MRATE_PPB, YDBI_CONFIG, &freq_offset_update_mrate_ppb, sizeof(freq_offset_update_mrate_ppb));
gptpgcfg_set_item(gpoptd.instnum, XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_STABLE_VALUE, YDBI_CONFIG, &phase_offset_iir_alpha_stable_value, sizeof(phase_offset_iir_alpha_stable_value));
gptpgcfg_set_item(gpoptd.instnum, XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_STABLE_VALUE, YDBI_CONFIG, &freq_offset_iir_alpha_stable_value, sizeof(freq_offset_iir_alpha_stable_value));
Limitations
For all parameters related to interval, the minimum interval can be configured for gPTP is 125ms. The reason for that minimum interval is the implementation uses a base timer which has minimum period is 125ms. Thus, increasing the interval parameters like sync-interval
which is not a multiple of 125ms may produce inaccurate interval of sending sync message.Or reducing interval of sync message below 125ms is not possible. And the same limitation applied for all remaining interval parameters.
See Also
Networking