IO-Link Master1.09.04

Overview

Acyclic Data API.

Functions

IOL_FUNC_DECL IOL_EErrorInfo IOLM_API_AL_eReadReq (INT8U u8Port_p, INT16U u16Index_p, INT8U u8Subindex_p)
 Send ISDU read request. More...
 
IOL_FUNC_DECL IOL_EErrorInfo IOLM_API_AL_eWriteReq (INT8U u8Port_p, INT16U u16Index_p, INT8U u8Subindex_p, INT8U *pu8Data_p, INT8U u8Length_p)
 Send ISDU write request. More...
 
IOL_FUNC_DECL void IOLM_API_AL_vAbort (INT8U u8Port_p)
 Abort a pending ISDU request. More...
 
IOL_FUNC_DECL void IOLM_Port_AL_vReadCnf (INT8U u8Port_p, INT16U u16ErrorInfo_p, const INT8U *pu8Data_p, INT8U u8Length_p)
 Read confirmation. More...
 
IOL_FUNC_DECL void IOLM_Port_AL_vWriteCnf (INT8U u8Port_p, INT16U u16ErrorInfo_p)
 Write confirmation. More...
 

Function Documentation

◆ IOLM_API_AL_eReadReq()

IOL_FUNC_DECL IOL_EErrorInfo IOLM_API_AL_eReadReq ( INT8U  u8Port_p,
INT16U  u16Index_p,
INT8U  u8Subindex_p 
)

Send ISDU read request.

The AL read request is used to trigger a read on the specified index and port. For index values >= 2 the ISDU channel is used. This requires a connected Device with ISDU support. Index 0 is used to access the Direct Parameter Page 1. Index 1 is used to access the Direct Parameter Page 2.

On success the function IOLM_Port_AL_vReadCnf is called if the service has finished.

For details see Annex B in IO-Link Specification v1.1.2.

Parameters
[in]u8Port_pThe port number of the affected port.
[in]u16Index_pISDU Index / 0 for DPP1 / 1 for DPP2.
[in]u8Subindex_pParameter SubIndex.
Returns
IOL_EErrorInfo ErrorCode
Precondition
The port number must be smaller than IOLM_PORT_COUNT.
Postcondition
On success no further call until IOLM_Port_AL_vReadCnf is called by stack.
IRQ-safe
No Function needs to be called in Mainloop context.

◆ IOLM_API_AL_eWriteReq()

IOL_FUNC_DECL IOL_EErrorInfo IOLM_API_AL_eWriteReq ( INT8U  u8Port_p,
INT16U  u16Index_p,
INT8U  u8Subindex_p,
INT8U pu8Data_p,
INT8U  u8Length_p 
)

Send ISDU write request.

The AL write request is used to trigger a write on the specified index and port. For Index values >= 2 the ISDU channel is used. This requires a connected Device with ISDU support. Index 1 is used to access the Direct Parameter Page 2.

On success the function IOLM_Port_AL_vWriteCnf is called if the service has finished.

Parameters
[in]u8Port_pThe port number of the affected port.
[in]u16Index_pISDU index / 1 for DPP2.
[in]u8Subindex_pParameter SubIndex
[in]pu8Data_pData to be written.
[in]u8Length_pLength of pu8Data_p.
Returns
IOL_EErrorInfo ErrorCode
Precondition
The port number must be smaller than IOLM_PORT_COUNT. Provide valid data.
Postcondition
On success, data is copied and has not to be kept valid.
IRQ-safe
No Function needs to be called in Mainloop context.

◆ IOLM_API_AL_vAbort()

IOL_FUNC_DECL void IOLM_API_AL_vAbort ( INT8U  u8Port_p)

Abort a pending ISDU request.

The AL abort cancels the pending read or write request and triggers the corresponding callback with ErrorCode IOL_eErrorType_SERV_NOTAVAIL.

Parameters
[in]u8Port_pThe port number of the affected port.
Precondition
The port number must be smaller than IOLM_PORT_COUNT.
Postcondition
None.
IRQ-safe
No Function needs to be called in Mainloop context.

◆ IOLM_Port_AL_vReadCnf()

IOL_FUNC_DECL void IOLM_Port_AL_vReadCnf ( INT8U  u8Port_p,
INT16U  u16ErrorInfo_p,
const INT8U pu8Data_p,
INT8U  u8Length_p 
)

Read confirmation.

This function is called if a read request is handled. If the error info is IOL_eErrorType_NONE, the data pointer is valid.

Parameters
[in]u8Port_pThe port number of the affected port.
[in]u16ErrorInfo_pError information (see IOL_EErrorType).
[in]pu8Data_pResponse data.
[in]u8Length_pResponse data Length.
Precondition
The port number must be smaller than IOLM_PORT_COUNT.
Postcondition
None.
IRQ-safe
No Function will be called from Mainloop context.

◆ IOLM_Port_AL_vWriteCnf()

IOL_FUNC_DECL void IOLM_Port_AL_vWriteCnf ( INT8U  u8Port_p,
INT16U  u16ErrorInfo_p 
)

Write confirmation.

This function is called if a write request is handled. If the error info is IOL_eErrorType_NONE, the write operation was successful.

Parameters
[in]u8Port_pThe port number of the affected port.
[in]u16ErrorInfo_pError information (see IOL_EErrorType).
Precondition
The port number must be smaller than IOLM_PORT_COUNT.
Postcondition
None.
IRQ-safe
No Function will be called from Mainloop context.