EtherNet/IP™ Adapter3.02.00
EI_API_ADP_SLldp_Parameter Struct Reference

Nonvolatile attribute parameter of LLDP Management object. More...

#include <EI_API_def.h>

Data Fields

uint16_t enableArrayLength
 
union {
   uint8_t   allBits
 
   struct {
      uint8_t   global_enable: 1
 
      uint8_t   port1_tx_enable: 1
 
      uint8_t   port2_tx_enable: 1
 
   } 
 
enableArray
 
uint16_t msgTxInterval
 
uint8_t msgTxHold
 

Detailed Description

Nonvolatile attribute parameter of LLDP Management object.