EtherNet/IP™ Adapter3.02.00
◆ EI_API_CIP_addClassAttr()
uint32_t EI_API_CIP_addClassAttr
(
T *
pCipNode_p ,
uint16_t
classId_p ,
EI_API_CIP_SAttr_t *
pAttr_p
)
Add an attribute to a class.
This function adds an attribute to a class with the class identifier passed in parameter classId
. The attribute parameter details are passed as a struct of type EI_API_CIP_SAttr_t
.
Parameters
[in] pCipNode_p Pointer to the CIP node.
[in] classId_p Class identifier.
[in] pAttr_p Pointer to struct of attribute parameters.
Returns EI_API_CIP_EError_t as uint32_t value.
Return values
Example #include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
See also EI_API_CIP_getClassAttr EI_API_CIP_setClassAttr EI_API_CIP_SAttr_t EI_API_CIP_EAr_t EI_API_CIP_EEdt_t EI_API_CIP_ECdt_t
EI_API_CIP_EEdt_t edt
Definition: EI_API_CIP_define.h:189
EI_API_CIP_ECdt_t cdt
Definition: EI_API_CIP_define.h:190
@ EI_API_CIP_eEDT_UINT
Definition: EI_API_CIP_define.h:123
General attribute parameter collection.
Definition: EI_API_CIP_define.h:186
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition: EI_API_CIP_stub.c:230
ETHIP_API uint32_t EI_API_CIP_addClassAttr(T *pCipNode_p, uint16_t classId_p, EI_API_CIP_SAttr_t *pAttr_p)
Add an attribute to a class.
Definition: EI_API_CIP_stub.c:451
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_stub.c:102
uint16_t cdtSize
Definition: EI_API_CIP_define.h:193
EI_API_CIP_EAr_t accessRule
Definition: EI_API_CIP_define.h:191
uint16_t id
Definition: EI_API_CIP_define.h:188
uint16_t edtSize
Definition: EI_API_CIP_define.h:192
@ EI_API_CIP_eCDT_NO
Definition: EI_API_CIP_define.h:158
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256
@ EI_API_CIP_eAR_GET
Attribute is gettable.
Definition: EI_API_def.h:130