uint32_t EI_API_ADP_setIntfConfig | ( | T * | pAdp_p, |
uint8_t | intfId_p, | ||
EI_API_ADP_UIntfConf_t | intfConf_p | ||
) |
Set the adapter Ethernet interface configuration (Instance Attribute ID: 6).
This function can be used to set the current adapter Ethernet interface configuration.
[in] | pAdp_p | Pointer to the adapter. |
[in] | intfId_p | Interface ID. |
intfConf_p | New interface configuration. |
EI_API_ADP_OK | Success. |
EI_API_ADP_ERROR | General error. |