EtherNet/IP™ Adapter3.02.00

◆ EI_API_ADP_init()

uint32_t EI_API_ADP_init ( T *  pAdp_p,
EI_API_ADP_SInit_t  params_p 
)

Apply parameters.

After the configuration of all device parameters of the adapter, the EI_API_ADP_init function is called to apply the parameters.

Parameters
[in]pAdp_pPointer to the adapter.
[in]params_pInitialization parameters.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
// create a new adapter
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
EI_API_ADP_SInit_t initParams = {0};
uint8_t numInterfaces = 1;
uint16_t vendorId = 806;
uint16_t deviceType = 0x000c;
uint16_t productCode = 25601;
uint32_t serialNumber = 0x00000065;
const char productName[] = "EtherNet/IP(tm) Adapter";
// Create a new adapter
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Make your adapter settings
errCode = EI_API_ADP_setVendorId(pEI_API_ADP, vendorId);
errCode = EI_API_ADP_setDeviceType(pEI_API_ADP, deviceType);
errCode = EI_API_ADP_setProductCode(pEI_API_ADP, productCode);
revision.major = 0x01;
revision.minor = 0x02;
errCode = EI_API_ADP_setRevision(pEI_API_ADP, revision);
errCode = EI_API_ADP_setSerialNumber(pEI_API_ADP, serialNumber);
errCode = EI_API_ADP_setProductName(pEI_API_ADP, productName);
initParams.taskPrioCyclicIo = OSAL_TASK_ePRIO_EIP_CYCLICIO;
initParams.taskPrioPacket = OSAL_TASK_ePRIO_EIP_PACKET;
initParams.taskPrioStatistic = OSAL_TASK_ePRIO_EIP_STATISTIC;
// Finally apply your settings
errCode = EI_API_ADP_init(pEI_API_ADP, initParams);
See also
EI_API_ADP_new EI_API_ADP_EError_t
EI_API_ADP_SInit::taskPrioCyclicIo
OSAL_TASK_EPriority_t taskPrioCyclicIo
Definition: EI_API_ADP_define.h:156
EI_API_ADP_setSerialNumber
ETHIP_API uint32_t EI_API_ADP_setSerialNumber(T *pAdp_p, uint32_t serialNumber_p)
Set the adapter's unique Serial Number (Instance Attribute ID: 6).
Definition: EI_API_ADP_stub.c:1207
EI_API_ADP_SInit::taskPrioPacket
OSAL_TASK_EPriority_t taskPrioPacket
Definition: EI_API_ADP_define.h:157
EI_API_ADP_SRevision::minor
uint8_t minor
Definition: EI_API_ADP_define.h:127
EI_API_ADP_setProductCode
ETHIP_API uint32_t EI_API_ADP_setProductCode(T *pAdp_p, uint16_t productCode_p)
Set the adapter Product Code (Instance Attribute ID: 3).
Definition: EI_API_ADP_stub.c:968
EI_API_ADP_SInit::taskPrioStatistic
OSAL_TASK_EPriority_t taskPrioStatistic
Definition: EI_API_ADP_define.h:158
EI_API_ADP_setVendorId
ETHIP_API uint32_t EI_API_ADP_setVendorId(T *pAdp_p, uint16_t vendorId_p)
Set the adapter Vendor ID (Instance Attribute ID: 1).
Definition: EI_API_ADP_stub.c:734
EI_API_ADP_setDeviceType
ETHIP_API uint32_t EI_API_ADP_setDeviceType(T *pAdp_p, uint16_t deviceType_p)
Set the adapter Device Type (Instance Attribute ID: 2).
Definition: EI_API_ADP_stub.c:854
EI_API_ADP_SRevision::major
uint8_t major
Definition: EI_API_ADP_define.h:125
EI_API_ADP_SInit
Definition: EI_API_ADP_define.h:154
EI_API_ADP_init
ETHIP_API uint32_t EI_API_ADP_init(T *pAdp_p, EI_API_ADP_SInit_t params_p)
Apply parameters.
Definition: EI_API_ADP_stub.c:400
EI_API_ADP_setRevision
ETHIP_API uint32_t EI_API_ADP_setRevision(T *pAdp_p, EI_API_ADP_SRevision_t revison_p)
Set the adapter Revision (Instance Attribute ID: 4).
Definition: EI_API_ADP_stub.c:1089
EI_API_ADP_SRevision
Definition: EI_API_ADP_define.h:123
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256
EI_API_ADP_setProductName
ETHIP_API uint32_t EI_API_ADP_setProductName(T *pAdp_p, const char *pProductName_p)
Set the adapter Product Name (Instance Attribute ID: 7).
Definition: EI_API_ADP_stub.c:1328