uint32_t EC_SLAVE_APP_assignmentChangedHandler | ( | void * | pContext_p, |
bool | rx_p, | ||
uint8_t | count_p, | ||
uint16_t * | pPdoIndexArray_p | ||
) |
Change on PDO assignment configuration.
[in] | pContext_p | The pointer to the EtherCAT API instance. |
[in] | rx_p | Change on RX or TX PDOs. |
[in] | count_p | Number of PDOs assigned to SyncManager. |
[in] | pPdoIndexArray_p | Array of PDO indexes assigned to SyncManager. |