uint32_t EC_SLAVE_APP_mappingChangedHandler | ( | void * | pContext_p, |
uint16_t | pdoIndex_p, | ||
uint8_t | count_p, | ||
EC_SLV_API_PDO_SEntryMap_t * | pPdoMap_p | ||
) |
Change on PDO mapping configuration.
[in] | pContext_p | The pointer to the EtherCAT API instance. |
[in] | pdoIndex_p | PDO index number. |
[in] | count_p | Number of objects mapped as PDO. |
[in] | pPdoMap_p | PDO mapping entries. |