EtherCAT Slave1.12.02

◆ EC_API_SLV_PDO_getData()

uint32_t EC_API_SLV_PDO_getData ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
EC_API_SLV_SPdo_t pPdo_p,
uint32_t  length_p,
uint8_t *  pData_p 
)

Read PDO content from Process Image, all entries are read in a data chunk.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pPdo_ppointer to PDO instance
[in]length_pdata length in bytes
[in]pData_ppointer to data
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
void* pvVariable = NULL;
// the Call
retVal = EC_API_SLV_PDO_getData(ptEcSlvApi, ptRxPdo, length, data);
uint32_t EC_API_SLV_PDO_getData(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SPdo_t *pPdo_p, uint32_t length_p, uint8_t *pData_p)
Read PDO content from Process Image, all entries are read in a data chunk.
Definition: ecSlvApi_ProcDataStub.c:363