EtherCAT Slave1.12.02

◆ EC_API_SLV_getOutputData()

uint32_t EC_API_SLV_getOutputData ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint32_t  length_p,
uint8_t *  pOutputData_p 
)

Read output process from the EtherCAT Master.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]length_pdata length in bytes
[in]pOutputData_ppointer to data
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
// the Call
retVal = EC_API_SLV_getOutputData(ptEcSlvApi, length, data);
uint32_t EC_API_SLV_getOutputData(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint32_t length_p, uint8_t *pOutputData_p)
Read output process from the EtherCAT Master.
Definition: ecSlvApi_ProcDataStub.c:1067