EtherCAT Slave1.12.02

◆ EC_API_SLV_getInputProcDataLength()

uint32_t EC_API_SLV_getInputProcDataLength ( EC_API_SLV_SHandle_t pEcSlaveApi_p)

Read the input process data length.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
Returns
Returns the input process data length.
Example
#include <ecSlvApi.h>
uint32_t length = EC_API_SLV_getInputProcDataLength(ptEcSlvApi);
uint32_t EC_API_SLV_getInputProcDataLength(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
Read the input process data length.
Definition: ecSlvApi_ProcDataStub.c:862
See also
EC_API_SLV_getOutputProcDataLength
Examples
ESL_cia402Demo.c.