EtherCAT Slave1.12.02

◆ EC_API_SLV_cbRegisterPhyLibDetect()

void EC_API_SLV_cbRegisterPhyLibDetect ( CUST_PHY_CBextPhyLibDetect_t  cbFunc_p,
void *  pContext_p 
)

Register an application specific Phy Library.

Parameters
[in]cbFunc_pPhy detection function.
[in]pContext_pApplication context for external PhyLib
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_cbRegisterPhyLibDetect(detectMyPhy, myPhyLibContext);
void EC_API_SLV_cbRegisterPhyLibDetect(CUST_PHY_CBextPhyLibDetect_t cbFunc_p, void *pContext_p)
Register an application specific Phy Library.
Definition: ecSlvApi_BoardStub.c:163
See also
EC_API_SLV_phyRegRead, EC_API_SLV_phyRegWrite