EtherCAT Slave1.12.02

◆ EC_API_SLV_cbRegisterPhyReset()

void EC_API_SLV_cbRegisterPhyReset ( CUST_PHY_CBreset_t  cbFunc_p,
void *  pContext_p 
)

This is the function to register Phy Reset Function.

Parameters
[in]cbFunc_pFunction pointer to the Phy Reset Handler.
[in]pContext_pCall context for PHY Reset.
Example
#include <ecSlvApi.h>
// the Call
retVal = void EC_API_SLV_cbRegisterPhyReset(cbFunc, NULL);
void EC_API_SLV_cbRegisterPhyReset(CUST_PHY_CBreset_t cbFunc_p, void *pContext_p)
This is the function to register Phy Reset Function.
Definition: ecSlvApi_BoardStub.c:79
Examples
ecSlvCiA402.c.