EtherCAT Slave1.12.02

◆ EC_API_SLV_getCyclicStatus()

uint32_t EC_API_SLV_getCyclicStatus ( EC_API_SLV_SHandle_t pEcSlaveApi_p)

This function reads if there is any error cyclic communication error.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
uint32_t EC_API_SLV_getCyclicStatus(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
This function reads if there is any error cyclic communication error.
Definition: ecSlvApiStub.c:946
enum EC_API_EError EC_API_EError_t