EtherCAT Slave1.12.02

◆ EC_API_SLV_setState()

uint32_t EC_API_SLV_setState ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
EC_API_SLV_EEsmState_t  state_p,
uint16_t  alErrorCode_p 
)

This is the function to request a EtherCAT state.

Parameters
[in]pEcSlaveApi_pSlave API Handle
[in]state_pState to set.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
EC_API_SLV_setState(ecSlaveApi, state_p);
uint32_t EC_API_SLV_setState(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_EEsmState_t state_p, uint16_t alErrorCode_p)
This is the function to request a EtherCAT state.
Definition: ecSlvApiStub.c:1067