EtherCAT Slave1.12.02

◆ EC_API_SLV_getConfigStatus()

uint32_t EC_API_SLV_getConfigStatus ( EC_API_SLV_SHandle_t pEcSlaveApi_p)

This function reads the EtherCAT driver status.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
uint32_t EC_API_SLV_getConfigStatus(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
This function reads the EtherCAT driver status.
Definition: ecSlvApiStub.c:908
enum EC_API_EError EC_API_EError_t