EtherCAT Slave1.12.02

◆ EC_API_SLV_enableMdioManualMode()

uint32_t EC_API_SLV_enableMdioManualMode ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint32_t  manualMdioAddress_p 
)

Enable mdio manual mode (TI workaround enable)

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]manualMdioAddress_pmanual mdio mode address register
Returns
error code
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_enableMdioManualMode(ecSlaveApi, MDIO_MANUAL_MODE_BASE_ADDRESS);
uint32_t EC_API_SLV_enableMdioManualMode(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint32_t manualMdioAddress_p)
Enable mdio manual mode (TI workaround enable)
Definition: ecSlvApiStub.c:1477