typedef uint32_t(* EC_API_SLV_PDO_CBMappingChanges_t) (void *pContext_p, uint16_t pdoIndex_p, uint8_t count_p, EC_SLV_API_PDO_SEntryMap_t *pPdoMap_p) |
Inform about PDO mapping changes.
[in] | pContext_p | Function context. |
[in] | pdoIndex_p | PDO index. |
[in] | count_p | Number of entries mapped into the PDO. |
[in] | pPdoMap_p | PDO mapping configuration array. |
EC_API_eERR_NONE | Allow PDO mapping changes. |
EC_API_eERR_ABORT | Refuse PDO mapping changes. |