EtherCAT Slave1.12.02

◆ EC_SLV_APP_transitionAction()

bool EC_SLV_APP_transitionAction ( int16_t  characteristic_p)

This function shall calculate the desired Axis input values to move on a predefined ramp.

Parameters
[in]characteristic_pRamp description.
Returns
bool True if transition finished.
Example
// required variables
int16_t characteristic
// the Call
retVal = EC_SLV_APP_transitionAction(characteristic);
bool EC_SLV_APP_transitionAction(int16_t characteristic_p)
This function shall calculate the desired Axis input values to move on a predefined ramp.
Definition: ESL_cia402Demo.c:560
Examples
ESL_cia402Demo.c.