EtherCAT Slave1.12.02

◆ EC_SLV_APP_CST()

void EC_SLV_APP_CST ( EC_SLV_APP_Sapplication_t pApplication_p,
EC_SLV_API_CiA402_SAxis_t pCiA402Axis_p,
bool  gotOffsets 
)

Cyclic synchronous torque mode. ETG6010 6.4.

Parameters
[in]pApplication_pApplication instance.
[in]pCiA402Axis_pServo Axis description structure.
[in]gotOffsetsgot offsets
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
EC_SLV_APP_CST(S_ecSlvApiHdl, pCiA402Axis);
void EC_SLV_APP_CST(EC_SLV_APP_Sapplication_t *pApplication_p, EC_SLV_API_CiA402_SAxis_t *pCiA402Axis_p, bool gotOffsets)
Cyclic synchronous torque mode. ETG6010 6.4.
Definition: ESL_cia402Demo.c:613
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:157
Data structure to handle an CiA 402 axis.
Definition: ESL_cia402Demo.c:65
Examples
ESL_cia402Demo.c.