EtherCAT-IOLink Gateway
GW_API_SPortStatus Struct Reference

typedef struct of GW_API_getPortStatus() data More...

#include <gw_api_interface.h>

Data Fields

uint16_t vendorID
 
uint32_t deviceID
 vendorId from connected device More...
 
uint8_t revisionID
 deviceId from connected device More...
 
uint8_t inputDataLength
 revisionId from connected device More...
 
uint8_t outputDataLength
 length of PDin More...
 
uint8_t serialNumber [GW_API_SERIALNR_LEN]
 length of PDout More...
 
uint8_t portQualityInfo
 serialnumber More...
 
uint8_t connectionQuality
 quality of port More...
 
uint8_t mseqCapability
 quality of connection More...
 
uint8_t portStatusInfo
 IODD 0x00:4. More...
 
uint8_t masterCycleTime
 mode of port, described in enum IOLM_SMI_EPortStatus More...
 

Detailed Description

typedef struct of GW_API_getPortStatus() data