AM64x MCU+ SDK  08.06.00
vsc8514.h File Reference

Introduction

This file contains the type definitions and helper macros for the VSC8514 Ethernet PHY.

Go to the source code of this file.

Data Structures

struct  Vsc8514_Cfg
 VSC8514 PHY configuration parameters. More...
 

Macros

#define VSC8514_LED_NUM   (4U)
 Number of LEDs available in the PHY. More...
 

Functions

void Vsc8514_initCfg (Vsc8514_Cfg *cfg)
 Initialize VSC8514 PHY specific config params. More...