Request for writing the entire keystore contents.
A user may unlock the keystore to write its contents using a signed and encrypted keystore structure. This operation is required for keystore initialization and is mandatorily the first keystore operation which must be executed in order to put the keystore in a valid state for subsequent operations.
- Parameters
-
hdr | Common TI-SCI header |
keystore_lo | Lower 32-bit memory location of the signed and encrypted keystore contents |
keystore_hi | Higher 32-bit memory location of the signed and encrypted keystore contents |