AM64x MCU+ SDK  08.06.00
RED_NODE_TABLE_ENTRY Struct Reference

Detailed Description

Node Table Entry.

Data Fields

uint8_t src [ETHER_ADDR_LEN]
 
uint8_t state
 
uint8_t status
 
uint32_t cntRxA
 
uint32_t cntRxB
 
uint32_t errRxA
 
uint32_t errRxB
 
uint8_t cntRxSupA
 
uint8_t cntRxSupB
 
uint16_t timeLasSeenS
 
uint16_t timeLasSeenA
 
uint16_t timeLasSeenB
 

Field Documentation

◆ src

uint8_t RED_NODE_TABLE_ENTRY::src[ETHER_ADDR_LEN]

Source Address (MAC address of the node)

◆ state

uint8_t RED_NODE_TABLE_ENTRY::state

Valid (1) / Invalid (0)

◆ status

uint8_t RED_NODE_TABLE_ENTRY::status

Duplicate Discard [8:7] and Node Type [5:0]

◆ cntRxA

uint32_t RED_NODE_TABLE_ENTRY::cntRxA

Frames received on port A

◆ cntRxB

uint32_t RED_NODE_TABLE_ENTRY::cntRxB

Frames received on port B

◆ errRxA

uint32_t RED_NODE_TABLE_ENTRY::errRxA

Erroneous frames received on port A

◆ errRxB

uint32_t RED_NODE_TABLE_ENTRY::errRxB

Erroneous frames received on port B

◆ cntRxSupA

uint8_t RED_NODE_TABLE_ENTRY::cntRxSupA

Number of supervision frames received on port A

◆ cntRxSupB

uint8_t RED_NODE_TABLE_ENTRY::cntRxSupB

Number of supervision frames received on port B

◆ timeLasSeenS

uint16_t RED_NODE_TABLE_ENTRY::timeLasSeenS

Time last seen of a supervision frame

◆ timeLasSeenA

uint16_t RED_NODE_TABLE_ENTRY::timeLasSeenA

Time last seen of a frame received on port A

◆ timeLasSeenB

uint16_t RED_NODE_TABLE_ENTRY::timeLasSeenB

Time last seen of a frame received on port B