AM64x MCU+ SDK  08.06.00

Introduction

This module contains APIs to program and use the PCIE module. The APIs can be used by other drivers to get access to PCIE and also by applications

Files

file  pcie/pcie.h
 PCIE Driver API/interface file.
 

Data Structures

struct  Pcie_DeviceCfgBaseAddr
 The Pcie_DeviceCfg is used to specify device level configuration of the driver instance. More...
 
struct  Pcie_ObAtuCfg
 Pcie_ObAtuCfg specifies the Outbound ATU configurations for PCIe. More...
 
struct  Pcie_IbAtuCfg
 Pcie_IbAtuCfg specifies the Inbound ATU configurations for PCIe. More...
 
struct  Pcie_RegisterMsiIsrParams
 Pcie_RegisterMsiIsrParams specifies the parameters to register an ISR for MSI. More...
 
struct  Pcie_RegisterMsixIsrParams
 Pcie_RegisterMsixIsrParams specifies the parameters to register an ISR for MSIX. More...
 
struct  Pcie_MsiIsrCtrl
 PCIe MSI Isr control structure. More...
 
struct  Pcie_MsixIsrCtrl
 ISR and arguement list for MSIx. More...
 
struct  Pcie_MsixTblEntry
 PCIe MSIx table entry. More...
 
struct  Pcie_MsixTbl
 
struct  Pcie_Attrs
 PCIe atributes. More...
 
struct  Pcie_Object
 PCIe driver object. More...
 
struct  Pcie_DeviceCfg
 PCIe device configuration. More...
 
struct  Pcie_InitCfg
 PCIe configuration for initalization. More...
 
struct  Pcie_Config
 PCIE global configuration array. More...
 
struct  Pcie_BarCfg
 PCIe BAR configuration info. More...
 
struct  Pcie_IbTransCfg
 Inbound traslation configuration info The Pcie_IbTransCfg is used to configure the Inbound Translation Registers. More...
 
struct  Pcie_AtuRegionParams
 This Structure defines the ATU region parameters. More...
 

Functions

void Pcie_init (void)
 This function initializes the PCIe module. More...
 
Pcie_Handle Pcie_open (uint32_t index)
 This function opens a given PCIe peripheral. More...
 
void Pcie_close (Pcie_Handle handle)
 Function to close PCIe peripheral specified by PCIe handle. More...
 
Pcie_DeviceCfgBaseAddrPcie_handleGetBases (Pcie_Handle handle)
 Get the device base address info for the PCIe peripheral. More...
 
int32_t Pcie_setInterfaceMode (Pcie_Handle handle, Pcie_Mode mode)
 Set interfac mode (RC/EP) More...
 
int32_t Pcie_getMemSpaceReserved (Pcie_Handle handle, uint32_t *resSize)
 Pcie_getMemSpaceReserved returns amount of reserved space between beginning of hardware's data area and the base returned by Pcie_getMemSpaceRange. More...
 
int32_t Pcie_getMemSpaceRange (Pcie_Handle handle, void **base, uint32_t *size)
 Returns the PCIe Internal Address Range for the memory space. This range is used for accessing memory. More...
 
int32_t Pcie_cfgBar (Pcie_Handle handle, const Pcie_BarCfg *barCfg)
 Configure a BAR Register (32 bits) More...
 
int32_t Pcie_atuRegionConfig (Pcie_Handle handle, Pcie_Location location, uint32_t atuRegionIndex, const Pcie_AtuRegionParams *atuRegionParams)
 Configure address translation registers. More...
 
int32_t Pcie_getVendorId (Pcie_Handle handle, Pcie_Location location, uint32_t *vendorId, uint32_t *deviceId)
 Get vendor ID and device ID of Pcie Device. More...
 
int32_t Pcie_waitLinkUp (Pcie_Handle handle)
 Wait for PCIe link training to complete. More...
 
int32_t Pcie_checkLinkParams (Pcie_Handle handle)
 Verify if the link parameters is established as configured. More...
 
int32_t Pcie_LtssmCtrl (Pcie_Handle handle, uint8_t enable)
 Enable/disable PCIe link training. More...
 
int32_t Pcie_setLanes (Pcie_Handle handle)
 Set number of PCIe lanes as configured. More...
 
int32_t Pcie_cfgEP (Pcie_Handle handle)
 Configure Pcie for EP (End Point) operation. PCIe mode setting is NOT done here (Pcie_setInterfaceMode) More...
 
int32_t Pcie_cfgRC (Pcie_Handle handle)
 Configure Pcie for RC (Root Complex) operation. PCIe mode setting is NOT done here (Pcie_setInterfaceMode) More...
 

Typedefs

typedef void * Pcie_Handle
 Driver handle returned by Pcie_open() call. More...
 
typedef void(* Pcie_MsiIsr) (void *arg, uint32_t msiData)
 Function pointer for the PCIe MSI ISR. More...
 
typedef void(* Pcie_MsixIsr) (void *arg, uint32_t msixData)
 Function pointer for the PCIe MSIx ISR. More...
 

Enumerations

enum  Pcie_Mode { PCIE_EP_MODE = 0, PCIE_LEGACY_EP_MODE, PCIE_RC_MODE }
 These are the possible values for PCIe mode. More...
 
enum  Pcie_Gen { PCIE_GEN1 = 1, PCIE_GEN2 = 2, PCIE_GEN3 = 3 }
 Enumeration for PCIE generations. More...
 
enum  Pcie_BarPref { PCIE_BAR_NON_PREF = 0, PCIE_BAR_PREF }
 These are the possible values for Prefetch BAR configuration. More...
 
enum  Pcie_BarType { PCIE_BAR_TYPE32 = 0, PCIE_BAR_RSVD, PCIE_BAR_TYPE64 }
 These are the possible values for Type BAR configuration. More...
 
enum  Pcie_BarMem { PCIE_BAR_MEM_MEM = 0, PCIE_BAR_MEM_IO }
 These are the possible values for Memory BAR configuration. More...
 
enum  Pcie_AtuRegionDir { PCIE_ATU_REGION_DIR_OUTBOUND, PCIE_ATU_REGION_DIR_INBOUND }
 Enum to select PCIe ATU(Address translation unit) region direction(Inbound or Outbound). This enum is used while configuring inbound or outbound region. More...
 
enum  Pcie_TlpType { PCIE_TLP_TYPE_MEM, PCIE_TLP_TYPE_IO, PCIE_TLP_TYPE_CFG }
 This enum is used to select PCIe TLP(Transaction layer packet) type while configuring inbound or outbound region. More...
 
enum  Pcie_AtuRegionMatchMode { PCIE_ATU_REGION_MATCH_MODE_ADDR, PCIE_ATU_REGION_MATCH_MODE_BAR }
 Enum to select address or BAR match mode. More...
 
enum  Pcie_Location { PCIE_LOCATION_LOCAL, PCIE_LOCATION_REMOTE }
 Enumeration for PCIe access type remote/local. More...
 
enum  Pcie_LtssmState {
  PCIE_LTSSM_DETECT_QUIET =0, PCIE_LTSSM_DETECT_ACT, PCIE_LTSSM_POLL_ACTIVE, PCIE_LTSSM_POLL_COMPLIANCE,
  PCIE_LTSSM_POLL_CONFIG, PCIE_LTSSM_PRE_DETECT_QUIET, PCIE_LTSSM_DETECT_WAIT, PCIE_LTSSM_CFG_LINKWD_START,
  PCIE_LTSSM_CFG_LINKWD_ACEPT, PCIE_LTSSM_CFG_LANENUM_WAIT, PCIE_LTSSM_CFG_LANENUM_ACEPT, PCIE_LTSSM_CFG_COMPLETE,
  PCIE_LTSSM_CFG_IDLE, PCIE_LTSSM_RCVRY_LOCK, PCIE_LTSSM_RCVRY_SPEED, PCIE_LTSSM_RCVRY_RCVRCFG,
  PCIE_LTSSM_RCVRY_IDLE, PCIE_LTSSM_L0, PCIE_LTSSM_L0S, PCIE_LTSSM_L123_SEND_EIDLE,
  PCIE_LTSSM_L1_IDLE, PCIE_LTSSM_L2_IDLE, PCIE_LTSSM_L2_WAKE, PCIE_LTSSM_DISABLED_ENTRY,
  PCIE_LTSSM_DISABLED_IDLE, PCIE_LTSSM_DISABLED, PCIE_LTSSM_LPBK_ENTRY, PCIE_LTSSM_LPBK_ACTIVE,
  PCIE_LTSSM_LPBK_EXIT, PCIE_LTSSM_LPBK_EXIT_TIMEOUT, PCIE_LTSSM_HOT_RESET_ENTRY, PCIE_LTSSM_HOT_RESET,
  PCIE_LTSSM_RCVRY_EQ0, PCIE_LTSSM_RCVRY_EQ1, PCIE_LTSSM_RCVRY_EQ2, PCIE_LTSSM_RCVRY_EQ3
}
 Enumeration for possible values for encoding LTSSM state. More...
 

Macros

#define PCIE_MAX_PERIPHS   (4U)
 Maximum PCIe devices supported by the driver. More...
 
#define PCIE_MAX_MSI_IRQ   (32U)
 Maximum PCIe MSI interrupts supported. More...
 
#define PCIE_MAX_MSIX_IRQ   (2048U)
 Maxmium number of MSIx interrupts supported. More...
 

Macro Definition Documentation

◆ PCIE_MAX_PERIPHS

#define PCIE_MAX_PERIPHS   (4U)

Maximum PCIe devices supported by the driver.

◆ PCIE_MAX_MSI_IRQ

#define PCIE_MAX_MSI_IRQ   (32U)

Maximum PCIe MSI interrupts supported.

◆ PCIE_MAX_MSIX_IRQ

#define PCIE_MAX_MSIX_IRQ   (2048U)

Maxmium number of MSIx interrupts supported.

Typedef Documentation

◆ Pcie_Handle

typedef void* Pcie_Handle

Driver handle returned by Pcie_open() call.

◆ Pcie_MsiIsr

typedef void(* Pcie_MsiIsr) (void *arg, uint32_t msiData)

Function pointer for the PCIe MSI ISR.

◆ Pcie_MsixIsr

typedef void(* Pcie_MsixIsr) (void *arg, uint32_t msixData)

Function pointer for the PCIe MSIx ISR.

Enumeration Type Documentation

◆ Pcie_Mode

enum Pcie_Mode

These are the possible values for PCIe mode.

Enumerator
PCIE_EP_MODE 

Required when setting the PCIe Mode to End Point using the Pcie_setInterfaceMode function

PCIE_LEGACY_EP_MODE 

Required when setting the PCIe Mode to Legacy End Point using the Pcie_setInterfaceMode function

PCIE_RC_MODE 

Required when setting the PCIe Mode to Root Complex using the Pcie_setInterfaceMode function

◆ Pcie_Gen

enum Pcie_Gen

Enumeration for PCIE generations.

Enumerator
PCIE_GEN1 

PCIe Gen1 for 2.5 GT/s speed

PCIE_GEN2 

PCIe Gen2 for 5.0 GT/s speed

PCIE_GEN3 

PCIe Gen3 for 8.0 GT/s speed

◆ Pcie_BarPref

These are the possible values for Prefetch BAR configuration.

Enumerator
PCIE_BAR_NON_PREF 

Non Prefetchable Region

PCIE_BAR_PREF 

Prefetchable Region

◆ Pcie_BarType

These are the possible values for Type BAR configuration.

Enumerator
PCIE_BAR_TYPE32 

32 bits BAR

PCIE_BAR_RSVD 

Reserved

PCIE_BAR_TYPE64 

64 bits BAR

◆ Pcie_BarMem

These are the possible values for Memory BAR configuration.

Enumerator
PCIE_BAR_MEM_MEM 

Memory BAR

PCIE_BAR_MEM_IO 

IO BAR

◆ Pcie_AtuRegionDir

Enum to select PCIe ATU(Address translation unit) region direction(Inbound or Outbound). This enum is used while configuring inbound or outbound region.

Enumerator
PCIE_ATU_REGION_DIR_OUTBOUND 

Select PCIe outbound region.

PCIE_ATU_REGION_DIR_INBOUND 

Select PCIe inbound region.

◆ Pcie_TlpType

This enum is used to select PCIe TLP(Transaction layer packet) type while configuring inbound or outbound region.

Enumerator
PCIE_TLP_TYPE_MEM 

MEM type is selected while doing memory transfer

PCIE_TLP_TYPE_IO 

IO type is selected while doing I/O transfer

PCIE_TLP_TYPE_CFG 

CFG type is selected while doing configuration access

◆ Pcie_AtuRegionMatchMode

Enum to select address or BAR match mode.

Enumerator
PCIE_ATU_REGION_MATCH_MODE_ADDR 

Inbound packets are filtered by address match mode

PCIE_ATU_REGION_MATCH_MODE_BAR 

Inbound packets are filtered by BAR match mode

◆ Pcie_Location

Enumeration for PCIe access type remote/local.

Selects whether to read/write local or remote PCIe registers. PCIe configuration registers are accessible locally and remotely

For PCIe application registers the access is always local

Enumerator
PCIE_LOCATION_LOCAL 

Access the local PCIe peripheral

PCIE_LOCATION_REMOTE 

Access the remote PCIe peripheral

◆ Pcie_LtssmState

Enumeration for possible values for encoding LTSSM state.

Enumerator
PCIE_LTSSM_DETECT_QUIET 

0x00

PCIE_LTSSM_DETECT_ACT 

0x01

PCIE_LTSSM_POLL_ACTIVE 

0x02

PCIE_LTSSM_POLL_COMPLIANCE 

0x03

PCIE_LTSSM_POLL_CONFIG 

0x04

PCIE_LTSSM_PRE_DETECT_QUIET 

0x05

PCIE_LTSSM_DETECT_WAIT 

0x06

PCIE_LTSSM_CFG_LINKWD_START 

0x07

PCIE_LTSSM_CFG_LINKWD_ACEPT 

0x08

PCIE_LTSSM_CFG_LANENUM_WAIT 

0x09

PCIE_LTSSM_CFG_LANENUM_ACEPT 

0x0a

PCIE_LTSSM_CFG_COMPLETE 

0x0b

PCIE_LTSSM_CFG_IDLE 

0x0c

PCIE_LTSSM_RCVRY_LOCK 

0x0d

PCIE_LTSSM_RCVRY_SPEED 

0x0e

PCIE_LTSSM_RCVRY_RCVRCFG 

0x0f

PCIE_LTSSM_RCVRY_IDLE 

0x10

PCIE_LTSSM_L0 

0x11

PCIE_LTSSM_L0S 

0x12

PCIE_LTSSM_L123_SEND_EIDLE 

0x13

PCIE_LTSSM_L1_IDLE 

0x14

PCIE_LTSSM_L2_IDLE 

0x15

PCIE_LTSSM_L2_WAKE 

0x16

PCIE_LTSSM_DISABLED_ENTRY 

0x17

PCIE_LTSSM_DISABLED_IDLE 

0x18

PCIE_LTSSM_DISABLED 

0x19

PCIE_LTSSM_LPBK_ENTRY 

0x1a

PCIE_LTSSM_LPBK_ACTIVE 

0x1b

PCIE_LTSSM_LPBK_EXIT 

0x1c

PCIE_LTSSM_LPBK_EXIT_TIMEOUT 

0x1d

PCIE_LTSSM_HOT_RESET_ENTRY 

0x1e

PCIE_LTSSM_HOT_RESET 

0x1f

PCIE_LTSSM_RCVRY_EQ0 

0x20

PCIE_LTSSM_RCVRY_EQ1 

0x21

PCIE_LTSSM_RCVRY_EQ2 

0x22

PCIE_LTSSM_RCVRY_EQ3 

0x23

Function Documentation

◆ Pcie_init()

void Pcie_init ( void  )

This function initializes the PCIe module.

◆ Pcie_open()

Pcie_Handle Pcie_open ( uint32_t  index)

This function opens a given PCIe peripheral.

Precondition
PCIe controlled has been initialized using Pcie_init()
Parameters
indexIndex of config to use in the Pcie_config array
Returns
A Pcie_Handle on success or a NULL on an error or if it has been opened already

◆ Pcie_close()

void Pcie_close ( Pcie_Handle  handle)

Function to close PCIe peripheral specified by PCIe handle.

Precondition
Pcie_open() has to be called first
Parameters
handlePcie_Handle retuned from Pcie_open()

◆ Pcie_handleGetBases()

Pcie_DeviceCfgBaseAddr* Pcie_handleGetBases ( Pcie_Handle  handle)

Get the device base address info for the PCIe peripheral.

Parameters
handlePcie_Handle returned from Pcie_open()
Returns
Pointer to the base address info structure if success, else returns NULL

◆ Pcie_setInterfaceMode()

int32_t Pcie_setInterfaceMode ( Pcie_Handle  handle,
Pcie_Mode  mode 
)

Set interfac mode (RC/EP)

Parameters
handlePcie_Handle for the instance
modeInterface mode (EP/EC)
Returns
SystemP_SUCCESS on successful; else error on failure

◆ Pcie_getMemSpaceReserved()

int32_t Pcie_getMemSpaceReserved ( Pcie_Handle  handle,
uint32_t *  resSize 
)

Pcie_getMemSpaceReserved returns amount of reserved space between beginning of hardware's data area and the base returned by Pcie_getMemSpaceRange.

Parameters
handlePcie_Handle for the instance
resSizePointer to return reserved space
Return values
SystemP_SUCCESSon successful; else error on failure

◆ Pcie_getMemSpaceRange()

int32_t Pcie_getMemSpaceRange ( Pcie_Handle  handle,
void **  base,
uint32_t *  size 
)

Returns the PCIe Internal Address Range for the memory space. This range is used for accessing memory.

Parameters
handlePcie_Handle for the instance
basePointer to return base address
sizePointer to return size
Returns
SystemP_SUCCESS on successful; else error on failure

◆ Pcie_cfgBar()

int32_t Pcie_cfgBar ( Pcie_Handle  handle,
const Pcie_BarCfg barCfg 
)

Configure a BAR Register (32 bits)

Parameters
handlePcie_Handle for the instance
barCfgBar configuration parameters
Returns
SystemP_SUCCESS on successful; else error on failure

◆ Pcie_atuRegionConfig()

int32_t Pcie_atuRegionConfig ( Pcie_Handle  handle,
Pcie_Location  location,
uint32_t  atuRegionIndex,
const Pcie_AtuRegionParams atuRegionParams 
)

Configure address translation registers.

Parameters
handlePcie_Handle for the instance
locationLocal or remote configuration space
atuRegionIndexAddress translation region index
atuRegionParamsAddress translation region parameters
Returns
SystemP_SUCCESS on successful; else error on failure

◆ Pcie_getVendorId()

int32_t Pcie_getVendorId ( Pcie_Handle  handle,
Pcie_Location  location,
uint32_t *  vendorId,
uint32_t *  deviceId 
)

Get vendor ID and device ID of Pcie Device.

Parameters
handlePcie_Handle returned by Pcie_open()
locationLocal or remote configuration space
vendorIdPointer to return vendor ID
deviceIdPointer to return device ID
Returns
SystemP_SUCCESS if successful; else error on failure

◆ Pcie_waitLinkUp()

int32_t Pcie_waitLinkUp ( Pcie_Handle  handle)

Wait for PCIe link training to complete.

Parameters
handlePcie_Handle returned by Pcie_open()
Returns
SystemP_SUCCESS if successful; else error on failure

◆ Pcie_checkLinkParams()

int32_t Pcie_checkLinkParams ( Pcie_Handle  handle)

Verify if the link parameters is established as configured.

Precondition
Link training needs to be completed
Parameters
handlePcie_Handle returned by Pcie_open()
Returns
SystemP_SUCCESS if successful; else error on failure

◆ Pcie_LtssmCtrl()

int32_t Pcie_LtssmCtrl ( Pcie_Handle  handle,
uint8_t  enable 
)

Enable/disable PCIe link training.

Parameters
handlePcie_Handle returned by Pcie_open()
enableEnable(1) / disable (0) link training
Returns
SystemP_SUCCESS if successful; else error on failure

◆ Pcie_setLanes()

int32_t Pcie_setLanes ( Pcie_Handle  handle)

Set number of PCIe lanes as configured.

Parameters
handlePcie_Handle returned by Pcie_open()
Returns
SystemP_SUCCESS if successful; else error on failure

◆ Pcie_cfgEP()

int32_t Pcie_cfgEP ( Pcie_Handle  handle)

Configure Pcie for EP (End Point) operation. PCIe mode setting is NOT done here (Pcie_setInterfaceMode)

Parameters
handlePcie_Handle returned by Pcie_open()
Returns
SystemP_SUCCESS if successful; else error on failure

◆ Pcie_cfgRC()

int32_t Pcie_cfgRC ( Pcie_Handle  handle)

Configure Pcie for RC (Root Complex) operation. PCIe mode setting is NOT done here (Pcie_setInterfaceMode)

Parameters
handlePcie_Handle returned by Pcie_open()
Returns
SystemP_SUCCESS if successful; else error on failure

Variable Documentation

◆ gPcieConfig

Pcie_Config gPcieConfig[]
extern

Externally defined driver configuration array.

◆ gPcieConfigNum

uint32_t gPcieConfigNum
extern

Externally defined driver configuration array size.