EtherNet/IP™ Adapter3.02.00

◆ EI_API_CIP_addAssemblyMember()

uint32_t EI_API_CIP_addAssemblyMember ( T *  pCipNode_p,
uint16_t  assemblyInstanceId_p,
uint16_t  classId_p,
uint16_t  instanceId_p,
uint16_t  attributeId_p 
)

Add an member to an assembly member list.

This function adds the given attribute to the given assembly instance.

Parameters
[in]pCipNode_pPointer to the CIP node.
[in]assemblyInstanceId_pAssembly instance identifier.
[in]classId_pClass identifier.
[in]instanceId_pInstance identifier.
[in]attributeId_pAttribute identifier.
Returns
EI_API_CIP_EError_t as uint32_t value.
Return values
EI_API_CIP_eERR_OKSuccess.
EI_API_CIP_eERR_NODE_INVALIDCIP node is invalid, possibly EI_API_CIP_NODE_new() was not called.
EI_API_CIP_eERR_INSTANCE_DOES_NOT_EXISTInstance does not exist in CIP node dictionary.
EI_API_CIP_eERR_ATTRIBUTE_DOES_NOT_EXISTAttribute does not exist in class or instance.
EI_API_CIP_eERR_ASSEMBLY_DOES_NOT_EXISTThe assembly with the given ID could not be found.
EI_API_CIP_eERR_ASSEMBLY_INVALID_ACCESSMODEAttempted to add a read only attribute to a writable assembly.
EI_API_CIP_eERR_ASSEMBLY_MAXLENGTH_EXCEEDEDThe total length of assemblies data exceeds the maximum connection size.
EI_API_CIP_eERR_MEMALLOCMemory allocation error.
EI_API_CIP_eERR_GENERALGeneral CIP error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
EI_API_CIP_NODE_T* pEI_API_CIP_NODE = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t classId;
uint16_t instanceId;
uint16_t attrId;
uint16_t assemblyInstanceId;
// Create a new adapter first
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Create a CIP node next
pEI_API_CIP_NODE = EI_API_CIP_NODE_new();
...
// Create class for holding data attributes
classId = 0x70;
errCode = EI_API_CIP_createClass(pEI_API_CIP_NODE, classId);
// Define services on defined class
service.callback = NULL;
errCode = EI_API_CIP_addClassService(pEI_API_CIP_NODE, classId, &service);
errCode = EI_API_CIP_addClassService(pEI_API_CIP_NODE, classId, &service);
// Create instance with ID = 1, under defined class
instanceId = 0x01;
errCode = EI_API_CIP_createInstance(pEI_API_CIP_NODE, classId, instanceId);
// Add attribute with ID = 0x300 (Vendor Specific Attribute ID Range)
// of type USINT and read-write access under the created instance 0x01
attrId = 0x300;
attr.id = attrId;
attr.cdtSize = 0;
errCode = EI_API_CIP_addInstanceAttr(pEI_API_CIP_NODE, classId, instanceId, &attr);
// Set value of instance attribute in the instance with ID = 0x01
uint8_t value = 0xFF;
attr.pvValue = &value;
errCode = EI_API_CIP_setInstanceAttr(pEI_API_CIP_NODE, classId, instanceId, &attr);
// Under pEI_API_CIP_NODE, create assembly instance with ID = 100, with read-write access
assemblyInstanceId = 0x64;
errCode = EI_API_CIP_createAssembly(pEI_API_CIP_NODE, assemblyInstanceId, EI_API_CIP_eAR_GET_AND_SET);
...
// Add assembly member
errCode = EI_API_CIP_addAssemblyMember(pEI_API_CIP_NODE, assemblyInstanceId, classId, instanceId, attrId);
See also
EI_API_CIP_createAssembly EI_API_CIP_getAssemblySize EI_API_CIP_getAssemblyData EI_API_CIP_setAssemblyData EI_API_CIP_SService_t EI_API_CIP_SAttr_t EI_API_CIP_EAr_t EI_API_CIP_EError_t
EI_API_CIP_SAttr::edt
EI_API_CIP_EEdt_t edt
Definition: EI_API_CIP_define.h:189
EI_API_CIP_SAttr::cdt
EI_API_CIP_ECdt_t cdt
Definition: EI_API_CIP_define.h:190
EI_API_CIP_SService::code
EI_API_CIP_ESc_t code
Definition: EI_API_CIP_define.h:176
EI_API_CIP_SService::getAttrAllResponseCnt
uint16_t getAttrAllResponseCnt
Definition: EI_API_CIP_define.h:177
EI_API_CIP_createAssembly
ETHIP_API uint32_t EI_API_CIP_createAssembly(T *pCipNode_p, uint16_t assemblyInstanceId_p, EI_API_CIP_EAr_t accessRule_p)
Create a new assembly instance.
Definition: EI_API_CIP_stub.c:4145
EI_API_CIP_SAttr
General attribute parameter collection.
Definition: EI_API_CIP_define.h:186
EI_API_CIP_createInstance
ETHIP_API uint32_t EI_API_CIP_createInstance(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p)
Creates a CIP instance.
Definition: EI_API_CIP_stub.c:774
EI_API_CIP_eEDT_USINT
@ EI_API_CIP_eEDT_USINT
Definition: EI_API_CIP_define.h:122
EI_API_CIP_createClass
ETHIP_API uint32_t EI_API_CIP_createClass(T *pCipNode_p, uint16_t classId_p)
Create a CIP class.
Definition: EI_API_CIP_stub.c:230
EI_API_CIP_addClassService
ETHIP_API uint32_t EI_API_CIP_addClassService(T *pCipNode_p, uint16_t classId_p, EI_API_CIP_SService_t *pService_p)
Add service/s to the class.
Definition: EI_API_CIP_stub.c:304
EI_API_CIP_SService
General service parameter collection.
Definition: EI_API_CIP_define.h:174
EI_API_CIP_NODE_new
ETHIP_API T * EI_API_CIP_NODE_new(void)
Create a new CIP node.
Definition: EI_API_CIP_stub.c:102
EI_API_CIP_eSC_SETATTRSINGLE
@ EI_API_CIP_eSC_SETATTRSINGLE
Definition: EI_API_def.h:117
EI_API_CIP_SAttr::pvValue
void * pvValue
Definition: EI_API_CIP_define.h:195
EI_API_CIP_eSC_GETATTRSINGLE
@ EI_API_CIP_eSC_GETATTRSINGLE
Definition: EI_API_def.h:116
EI_API_CIP_SAttr::cdtSize
uint16_t cdtSize
Definition: EI_API_CIP_define.h:193
EI_API_CIP_SAttr::accessRule
EI_API_CIP_EAr_t accessRule
Definition: EI_API_CIP_define.h:191
EI_API_CIP_SAttr::id
uint16_t id
Definition: EI_API_CIP_define.h:188
EI_API_CIP_setInstanceAttr
ETHIP_API uint32_t EI_API_CIP_setInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Set instance attribute value only.
Definition: EI_API_CIP_stub.c:1432
EI_API_CIP_eCDT_NO
@ EI_API_CIP_eCDT_NO
Definition: EI_API_CIP_define.h:158
EI_API_CIP_addAssemblyMember
ETHIP_API uint32_t EI_API_CIP_addAssemblyMember(T *pCipNode_p, uint16_t assemblyInstanceId_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attributeId_p)
Add an member to an assembly member list.
Definition: EI_API_CIP_stub.c:4266
EI_API_CIP_eAR_GET_AND_SET
@ EI_API_CIP_eAR_GET_AND_SET
Definition: EI_API_def.h:131
EI_API_CIP_SService::callback
EI_API_CIP_CBService callback
Definition: EI_API_CIP_define.h:179
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256
EI_API_CIP_addInstanceAttr
ETHIP_API uint32_t EI_API_CIP_addInstanceAttr(T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, EI_API_CIP_SAttr_t *pAttr_p)
Add an attribute to an instance.
Definition: EI_API_CIP_stub.c:1032