EtherNet/IP™ Adapter3.02.00

◆ EI_API_ADP_getPtpEnable()

uint32_t EI_API_ADP_getPtpEnable ( T *  pAdp_p,
bool *  pPtpEnable_p 
)

Get the PTPEnable attribute of the Time Sync Object (Instance Attribute ID: 1).

Function that returns the PTPEnable attribute of the adapter selected by parameter pAdp_p in output parameter pPtpEnable.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pPtpEnable_pPointer to a boolean that is set to true if PTP is enabled and false if not.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
bool ptpEnable;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getPtpEnable(pEI_API_ADP, &ptpEnable);
See also
EI_API_ADP_setPtpEnable EI_API_ADP_EError_t
EI_API_ADP_getPtpEnable
ETHIP_API uint32_t EI_API_ADP_getPtpEnable(T *pAdp_p, bool *pPtpEnable_p)
Get the PTPEnable attribute of the Time Sync Object (Instance Attribute ID: 1).
Definition: EI_API_ADP_stub.c:1505
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256