EtherNet/IP™ Adapter3.02.00

◆ EI_API_ADP_getIpGateway()

uint32_t EI_API_ADP_getIpGateway ( T *  pAdp_p,
uint32_t *  pIpGateway_p 
)

Get the IP address of the default gateway (Instance Attribute ID: 5).

Function that returns the IP address of the default gateway of the adapter selected by parameter pAdp_p in output parameter pIpGateway_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pIpGateway_puint32_t pointer to gateway address for the adapter specified by parameter pAdp_p.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint32_t ipGateway;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getIpGateway(pEI_API_ADP, &ipGateway);
See also
EI_API_ADP_EError_t
EI_API_ADP_getIpGateway
ETHIP_API uint32_t EI_API_ADP_getIpGateway(T *pAdp_p, uint32_t *pIpGateway_p)
Get the IP address of the default gateway (Instance Attribute ID: 5).
Definition: EI_API_ADP_stub.c:3072
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256