EtherNet/IP™ Adapter3.02.00

◆ EI_API_ADP_getMcastConfiguration()

uint32_t EI_API_ADP_getMcastConfiguration ( T *  pAdp_p,
EI_API_ADP_SMcastConfig_t pMcastConfig_p 
)

Get the current Mcast configuration (Instance Attribute ID: 9).

Function that returns the current Mcast configuration for the adapter specified by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pMcastConfig_pPointer to structure of type EI_API_ADP_SMcastConfig_t which contains the Mcast configuration.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getMcastConfiguration(pEI_API_ADP, &mcastConfig);
See also
EI_API_ADP_setMcastConfiguration EI_API_ADP_SMcastConfig_t EI_API_ADP_EError_t
EI_API_ADP_getMcastConfiguration
ETHIP_API uint32_t EI_API_ADP_getMcastConfiguration(T *pAdp_p, EI_API_ADP_SMcastConfig_t *pMcastConfig_p)
Get the current Mcast configuration (Instance Attribute ID: 9).
Definition: EI_API_ADP_stub.c:3535
EI_API_ADP_SMcastConfig
General multi-cast attribute parameter collection.
Definition: EI_API_def.h:239
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256