EtherNet/IP™ Adapter3.02.00

◆ EI_API_ADP_setQuickConnectSupported()

uint32_t EI_API_ADP_setQuickConnectSupported ( T *  pAdp_p)

Enable QuickConnect support.

Enable QuickConnect support. This function should only be used for EtherNet/IP QuickConnect applications.

Parameters
[in]pAdp_pPointer to the adapter.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Enable QuickConnect
errCode = EI_API_ADP_setQuickConnectSupported(pEI_API_ADP);
See also
EI_API_ADP_getQuickConnectEnabled EI_API_ADP_setQuickConnectEnabled EI_API_ADP_EError_t
EI_API_ADP_setQuickConnectSupported
ETHIP_API uint32_t EI_API_ADP_setQuickConnectSupported(T *pAdp_p)
Enable QuickConnect support.
Definition: EI_API_ADP_stub.c:4115
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256