EtherNet/IP™ Adapter3.02.00

◆ EI_API_ADP_getDomainName()

uint32_t EI_API_ADP_getDomainName ( T *  pAdp_p,
char *  pDomainName_p 
)

Get the domain name (Instance Attribute ID: 5).

Function that returns a pointer to the domain name of the adapter selected by parameter pAdp_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pDomainName_pCharacter array with domain name.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char aDomainName[49];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getDomainName(pEI_API_ADP, aDomainName);
See also
EI_API_ADP_EError_t
EI_API_ADP_getDomainName
ETHIP_API uint32_t EI_API_ADP_getDomainName(T *pAdp_p, char *pDomainName_p)
Get the domain name (Instance Attribute ID: 5).
Definition: EI_API_ADP_stub.c:3244
EI_API_ADP_new
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_stub.c:256