EtherCAT Slave
1.12.02
◆
EC_API_SLV_getProductCode()
uint32_t EC_API_SLV_getProductCode
(
EC_API_SLV_SHandle_t
*
pEcSlaveApi_p
)
Get device product code.
Get device product code. Used by the Object Dictionary
Parameters
[in]
pEcSlaveApi_p
The pointer to the EtherCAT API instance.
Returns
uint32_t Returns the product code.
Example
#include <ecSlvApi.h>
EC_API_SLV_SHandle_t
* S_ecSlvApiHdl;
uint32_t productCode = 0;
// the Call
productCode =
EC_API_SLV_getProductCode
(S_ecSlvApiHdl);
EC_API_SLV_getProductCode
uint32_t EC_API_SLV_getProductCode(EC_API_SLV_SHandle_t *pEcSlaveApi_p)
Get device product code.
Definition:
ecSlvApi_ParamStub.c:781
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition:
ecSlvApi.h:157
See also
EC_API_SLV_setProductCode
Parameter Configuration
generated by
1.9.1