#include <theHeader.h>
uint32_t retVal = 0;
void* pvVariable = NULL;
void EC_API_SLV_cbRegisterBoardStatusLed(EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBBoardStatusLed_t cbFunc_p, void *pLedContext_p)
Register Board Status LED callback.
Definition: ecSlvApi_BoardStub.c:273
void(* EC_API_SLV_CBBoardStatusLed_t)(void *pContext_p, void *pLedContext_p, bool errLed_p, bool statusLed_p)
Set Status LED call back.
Definition: ecSlvApi.h:997
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:157