Specifies the specifies the network and protocol address of each port of the device (e.g. IP address). The Network Protocol specifies the protocol for the network.
Data Fields | |
uint16_t | portNumber |
uint16_t | networkProtocol |
uint16_t | addressSize |
uint8_t | portProtocolAddress [16] |
uint16_t portProtAddr_t::portNumber |
uint16_t portProtAddr_t::networkProtocol |
uint16_t portProtAddr_t::addressSize |
uint8_t portProtAddr_t::portProtocolAddress[16] |