Specifies the physical protocol and physical address (e.g. IEEE 802.3) of each port of the device (e.g. MAC address). The maximum number of characters is 16. Unused array elements are zero-filled.
Data Fields | |
uint8_t | physicalProtocol [16] |
uint16_t | sizeOfAddress |
uint8_t | portPhysicalAddress [16] |
uint8_t portPhysAddr_t::physicalProtocol[16] |
uint16_t portPhysAddr_t::sizeOfAddress |
uint8_t portPhysAddr_t::portPhysicalAddress[16] |