Input args for ENET_MDIO_IOCTL_C45_WRITE command.
Clause-45 register write arguments.
Data Fields | |
EnetMdio_Group | group |
uint32_t | phyAddr |
EnetMdio_C45Mmd | mmd |
uint16_t | reg |
uint16_t | val |
EnetMdio_Group EnetMdio_C45WriteInArgs::group |
User channel to be used to perform the register access
uint32_t EnetMdio_C45WriteInArgs::phyAddr |
PHY address
EnetMdio_C45Mmd EnetMdio_C45WriteInArgs::mmd |
MMD
uint16_t EnetMdio_C45WriteInArgs::reg |
Register address
uint16_t EnetMdio_C45WriteInArgs::val |
Value to be written