This structure is used for the actual used communication parameters. More...
#include <IOLM_Types.h>
Data Fields | |
IOL_ETargetMode | eTargetMode |
This parameter indicates the real operational mode of the port. | |
IOL_EBaudrate | eRealBaudrate |
This parameter indicates the real transmission rate. | |
INT8U | u8RealCycleTime |
This parameter contains the real cycle time. See Annex B.1.3 of IO-Link Specification v1.1.2. | |
INT8U | u8RealRevisionID |
This parameter indicates the real IO-Link revision ID. See Annex B.1.5 of IO-Link Specification v1.1.2. | |
INT8U | au8RealVendorID [2] |
This parameter indicates the real Vendor ID. | |
INT8U | au8RealDeviceID [3] |
This parameter indicates the real Device ID. | |
INT8U | au8RealFunctionID [2] |
This parameter indicates the real Function ID. | |
INT8U | au8RealSerialNumber [16] |
This parameter indicates the real Serial Number. | |
INT8U | u8RealSerialNumberLen |
This parameter indicates the real Serial Number length. | |
INT8U | u8PdInLength |
Actual input data length in number of bytes. | |
INT8U | u8PdOutLength |
Actual output data length in number of bytes. | |
This structure is used for the actual used communication parameters.