This structure is obsolete. It used for the wireless Master configuration before V1.1.3 release. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
INT16U | u16ArgBlockID |
Big endian. | |
INT8U | u8MasterID |
1 - 29. | |
INT8U | u8AHTEnable |
0 = disabled, 1 = enabled. | |
INT8U | au8Blacklist [10] |
INT16U | u16PairingTimeout |
Pairing timeout in seconds. | |
This structure is obsolete. It used for the wireless Master configuration before V1.1.3 release.
The ArgBlockID(IOLM_SMI_EArgBlockID) for this struct is IOLM_SMI_eArgBlockID_WMasterConfig = 0x0200.