This structure follows the IOLM_SMI_SHeader struct. More...
#include <IOLM_SMI_Types.h>
Data Fields | |
INT8U * | pu8ArgBlock |
Data buffer (can be NULL if u16ArgBlockLengthMax = 0). | |
INT16U | u16ArgBlockLength |
Used length of pu8ArgBlock. | |
INT16U | u16ArgBlockLengthMax |
Total memory Length of pu8ArgBlock. | |
INT16U | u16ExpRefArgBlockId |
Expected Response or referenced ArgBlock Id (0 = not used). | |
This structure follows the IOLM_SMI_SHeader struct.
pu8ArgBlock points to the data. u16ArgBlockLength is used to tell the recipient the used length of the ArgBlock. u16ArgBlockLengthMax defines the maximum length of the ArgBlock and can be bigger than u16ArgBlockLength, if a bigger answer is expected.