This structure defines Data Storage objects. More...
#include <IOLM_Types.h>
Data Fields | |
INT8U | au8Index [2] |
INT8U | u8Subindex |
INT8U | u8Length |
INT8U | au8Data [4] |
This structure defines Data Storage objects.
The structure can be used on non aligned buffer. Because of this, there are only byte values defined. The data field is only a dummy value and it's real length depends on the content.