EtherNet/IP™ Adapter  2.01.00
EI_API_ADP_SCmgrForwardOpenInfo Struct Reference

Definition for ConnectionManager callback functions. More...

#include <EI_API_def.h>

Data Fields

uint8_t prioTimeTick
 
uint8_t timeOutTicks
 
uint32_t o2tNwConId
 
uint32_t t2oNwConId
 
uint16_t conSerialNum
 
uint16_t orgVendorId
 
uint32_t orgSerialNum
 
uint8_t timeOutMulti
 
uint32_t o2tRPI
 
uint32_t o2tConPara
 
uint32_t t2oRPI
 
uint16_t t2oConPara
 
uint8_t typeTrigger
 
uint8_t conPathSize
 
uint8_t conPath [80]
 

Detailed Description

Definition for ConnectionManager callback functions.

Information from the ForwardOpen, LargeForwardOpen or ForwardClose message