EtherNet/IP™ Adapter  2.01.00

◆ EI_API_ADP_setPtpEnable()

uint32_t EI_API_ADP_setPtpEnable ( T *  pAdp_p,
bool  ptpEnable_p 
)

Enable or disable PTP functionality in the Time Sync Object of the current adapter (Instance Attribute ID: 1).

Function that sets the Time Sync object's PTP state.

Note
Note that EI_API_ADP_setPtpEnable() updates the the PTPEnable attribute value only in volatile memory. To update PTPEnable both in volatile and non-volatile memory use CIP service Set_Attribute_Single.
Parameters
[in]pAdp_pPointer to the adapter.
[in]ptpEnable_pTime Sync PTP state.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
// Set PTP enable in Time Sync object
errCode = EI_API_ADP_setPtpEnable(pEI_API_ADP, true);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_setPtpEnable(T *pAdp_p, bool ptpEnable_p)
Enable or disable PTP functionality in the Time Sync Object of the current adapter (Instance Attribut...
Definition: EI_API_ADP_main.c:2012
See also
EI_API_ADP_getPtpEnable EI_API_ADP_EError_t