EtherNet/IP™ Adapter  2.01.00

◆ EI_API_ADP_getTimeSyncManufactureID()

uint32_t EI_API_ADP_getTimeSyncManufactureID ( T *  pAdp_p,
char *  pManufactureID_p 
)

Get the ManufactureIdentity attribute of the Time Sync Object (Instance Attribute ID: 20).

Function that returns the ManufactureIdentity attribute of the Time Sync Object for the adapter selected by parameter pAdp_p in output parameter pManufactureID_p.

Parameters
[in]pAdp_pPointer to the adapter.
[out]pManufactureID_pchar pointer to ManufactureIdentity of the adapter Time Sync object specified by parameter pAdp_p.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
char manufactureID[4];
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_getTimeSyncManufactureID(pEI_API_ADP, manufactureID);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:301
ETHIP_API uint32_t EI_API_ADP_getTimeSyncManufactureID(T *pAdp_p, char *pManufactureID_p)
Get the ManufactureIdentity attribute of the Time Sync Object (Instance Attribute ID: 20).
Definition: EI_API_ADP_main.c:2620
See also
EI_API_ADP_setTimeSyncManufactureID EI_API_ADP_EError_t